Skip to main content
Senior III
Jan 29, 2026 12:39 PM UTC
Solved

HAL ADC DMA & UART variable casting question

NUCLEO-F411RE

I have ADC1 to DMA in a circular buffer 4 samples long (ADC_VAL). I then use a TIM1 interrupt to send the contents via UART to a PC.

int16_t ADC_VAL[4];
...
HAL_ADC_STart_DMA(&hadc1, (uint32_t *)ADC_VAL, 4);


/* TIM1 callback */
void HAL_TIM_periodElapsedCallback(TIM_HandleTypeDef *htim)
{
 HAL_UART_Transmit(&huart2, (uint8_t *)ADC_VAL, 16, 10);
}

 

Should I have declared ADC_VAL as a uint32_t ?

 

TDK
TDKBest answer
Jan 29, 2026 2:03 PM UTC

> Should I have declared ADC_VAL as a uint32_t ?

In general, no. ADC only needs a uint16_t to store content. Ensure your DMA is set up to half-word size.

> int16_t ADC_VAL[4];

This is an array of 4 uint16_t values, which is a total of 8 bytes, not 16.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

ST Technical Moderator
Jan 29, 2026 1:28 PM UTC

Hello @NicRoberts 

Please refer to the example below which use __IO uint16_t variable when calling HAL_ADC_Start_DMA().

STM32CubeF4/Projects/STM32F4-Discovery/Examples/ADC/ADC_RegularConversion_DMA at master · STMicroelectronics/STM32CubeF4

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Senior III
Jan 29, 2026 1:43 PM UTC

Thanks for the reply, maybe I wasn't being clear enough in the OP.

In the example you linked to (and similarly in my own code) we have

HAL_ADC_Start_DMA(&AdcHandle, (uint32_t*)&uhADCxConvertedValue, 1)

 

where uhADCxConvertedValue  is first declared as 16 bit then cast as 32 bit for the DMA. What is the size of uhADCxConvertedValue in memory?

Is it 16 bits of actual values from the ADC padded with 16 bits of 0s?
or

is it 16 bits? 

I ask as I need to know when transmitting the bytes via UART i.e. If its 16 then I just need 2 bytes...

Does that make sense?

TDK
TDKBest answer
Jan 29, 2026 2:03 PM UTC

> Should I have declared ADC_VAL as a uint32_t ?

In general, no. ADC only needs a uint16_t to store content. Ensure your DMA is set up to half-word size.

> int16_t ADC_VAL[4];

This is an array of 4 uint16_t values, which is a total of 8 bytes, not 16.

"If you feel a post has answered your question, please click ""Accept as Solution""."