Skip to main content
Associate
Dec 19, 2025 11:52 AM UTC
Question

H723 problems with ping (ETH+LWIP)

I'm trying to ping my NUCLEO-H723ZG board and I've failed with every attempt over many hours;

  • Nucleo board is connected to my MacBook over USB + ethernet cable with an ethernet adapter
  • I'm using STM32CubeMX with VSC extension (this setup works, I am able to program the board and debug it)

 

My goal: Ping the STM32 over ethernet 

Results:

Request timeout for icmp_seq 301
ping: sendto: Host is down

Or it will hardfault

 

Code:

/* USER CODE BEGIN PV */
extern struct netif gnetif;
/* USER CODE END PV */
...
/* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 /* USER CODE BEGIN 3 */
 ethernetif_input(&gnetif);
 sys_check_timeouts();
 }
 /* USER CODE END 3 */

Config:

These config files are based from .ioc files from this thread: https://community.st.com/t5/stm32-mcus-embedded-software/h723-ethernet-lwip-ping-problem/m-p/758419#M58561  (No help from linked topic helped here)

I've also tried this tutorial with the same results: https://rafalbartoszak.com/stm32-ethernet-the-first-launch/ 

Screenshot 2025-12-19 at 12.46.14.png

Screenshot 2025-12-19 at 12.46.33.png

Screenshot 2025-12-19 at 12.46.57.png

Screenshot 2025-12-19 at 12.47.21.png

Screenshot 2025-12-19 at 12.47.44.png

Screenshot 2025-12-19 at 12.47.57.png

 

4 replies

mbarg.1
Senior III
Dec 20, 2025 8:12 AM UTC

You have multiple problems with ICMP_packet_processing.c code.

Also calls to HAL drivers are not properly scheduled.

ten_filipAuthor
Associate
Dec 20, 2025 8:16 AM UTC

@mbarg.1 Would you please care to elaborate? I have no ICMP_packet_processing.c file, nor have I shown any HAL driver scheduling. 

mbarg.1
Senior III
Dec 20, 2025 8:53 AM UTC

Which software is running ethernet connection ? 

ST Employee
Dec 22, 2025 4:04 PM UTC

Hello @ten_filip, and welcome to ST community!

After reviewing your screenshots, I noticed several crucial configuration steps were missed for the Ethernet to work properly. Notably:

  • MPU configuration for Ethernet buffers and descriptors
  • Insufficient LwIP MEM_SIZE

I suggest following the example project LwIP_TCP_Echo_Server. For MPU configuration, enable both I-Cache and D-Cache, and apply the recommended settings.

STackPointer64_0-1766418792074.png

Additionally, add the following memory section declarations for Ethernet descriptors and buffers in the STM32H723ZGTX_FLASH.ld linker file to ensure proper placement and alignment with the MPU configuration.

STackPointer64_1-1766418848521.png

Finally, increase the heap memory allocation by modifying the memory size definition inside lwipopts.h.

STackPointer64_2-1766419314122.png

 

Please apply these changes and let me know how it goes.

Best regards,

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.