Skip to main content
JojoS
Associate III
Nov 8, 2024 7:55 PM UTC
Solved

H7 SystemInit contains line with no effect

I had debugging problems with a H7 target, and by stepping thru the boot process I found the following line in SystemInit():

 

/*
 * Disable the FMC bank1 (enabled after reset).
 * This, prevents CPU speculation access on this bank which blocks the use of FMC during
 * 24us. During this time the others FMC master (such as LTDC) cannot use it!
 */
 FMC_Bank1_R->BTCR[0] = 0x000030D2;

 

At this stage of the boot process, the FMC power is not enabled, and thus reading or writing the register has no effect. Am I overseeing something or is this line for confusion?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 8, 2024 8:03 PM UTC

Hello @JojoS ,


@JojoS wrote:

At this stage of the boot process, the FMC power is not enabled, 


You mean FMC clock not the power but your comment makes sense as the FMC clock is enabled in SystemInit_ExtMemCtl(), just after. 

I will escalate this remark internally and get back to you as soon as I have an answer. Internal ticket number for follow up: 196021

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 8, 2024 8:03 PM UTC

Hello @JojoS ,


@JojoS wrote:

At this stage of the boot process, the FMC power is not enabled, 


You mean FMC clock not the power but your comment makes sense as the FMC clock is enabled in SystemInit_ExtMemCtl(), just after. 

I will escalate this remark internally and get back to you as soon as I have an answer. Internal ticket number for follow up: 196021

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
JojoS
JojoSAuthor
Associate III
Nov 8, 2024 10:05 PM UTC

Thanks, of corse it as a minor issue as it should have no affect. But it would be clearer if it is conditionally inserted. 

mƎALLEm
ST Technical Moderator
Nov 13, 2024 2:12 PM UTC

FYI,

Issue confirmed and will be fixed.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
Nov 8, 2024 8:05 PM UTC

>> Am I overseeing something or is this line for confusion?

Are you easily confused, is it a problem?

Probably there due to the generic way in which ST builds these thing, and perhaps salient to one particular case.

Perhaps so when built as a secondary application the loader has already started the clocks, external memories, etc prior to getting here.

Which file/project was this lifted from? An EVAL / DISCO board?

The SystemInit() in ARM's model would be used to bring up the whole board and memories so startup.s code can copy statics, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..