Skip to main content
HTiwa.3
Visitor II
Jan 1, 2023 1:53 PM UTC
Question

Getting started with analog, STM32F769I-DISCO. undefined reference to wm8994_drv

I am trying this example on my STM32F769I-DISCO. I followed the given tutorial for adding the dependecy. wm8994 is in ../Components/wm8994/wm8994.h.

But when building the code I am getting

../stm32disco/test2_audioread/Debug/../Core/Src/main.c:1263: undefined reference to `wm8994_drv'

Tutorial link : https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_analog

Edit: When I looked the header file it is defined as extern. So it may be a problem how it can be resolved.

/* Audio driver structure */

extern AUDIO_DrvTypeDef   wm8994_drv;

#endif /* __WM8994_H */

This topic has been closed for replies.

1 reply

ST Technical Moderator
Jan 2, 2023 8:05 AM UTC

Hello @HTiwa.3​ ,

Make sure your project contains the include libraries pathing set up correctly with the dependencies.

So, you need to set up correctly the "Include Paths" for the project.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks