Skip to main content
Alessandro Greco
Associate
Mar 18, 2018 3:44 PM UTC
Question

Get signal from 2 or more FSR sensor with ADC - STM32F4DISCOVERY

Posted on March 18, 2018 at 16:44

Hi guys, i'm looking to get signal from ♯ FSR sensors with my STM32F4-Discovery. I set PA1 as ADC1_IN1 and after i associated DMA (with STM32CubeMX, HAL driver). So i generated the project and edited with System Workbench for STM32, added an int variable (fsrValue[1]) and in main, i started HAL_ADC_Start_DMA(&hadc1, fsrValue, 1);. It works fine but now i don't know how implement this for 2 or more FSR sensor, i tried to set PA2 with ADC1_IN2 and with ADC2_IN1 but without any results (only signal noise, tested with STM32 Studio,  even if i don't touch the second FSR). Is possible to have an example? Thanks!

PS: i used this video as tutorial:

https://www.youtube.com/watch?v=Q2McPYfevwo

 

See the attachment for the full project

#hal-adc #fsr-sensor #stm32f4discovery
This topic has been closed for replies.

1 reply

Visitor II
Apr 8, 2024 10:48 AM UTC

Hi Alessandro,

Did you manage to solve the problem?

Thanks.