Skip to main content
waldin80
Associate III
July 28, 2010
Question

Function of BOOT

  • July 28, 2010
  • 3 replies
  • 1078 views
Posted on July 28, 2010 at 16:21

Function of BOOT

#bootloader
This topic has been closed for replies.

3 replies

swhite2
Associate II
May 17, 2011
jpeacock23
Associate
May 17, 2011
Posted on May 17, 2011 at 14:00

After a reset the BOOT pins determine what section of memory is used for startup.  You can select user flash, system bootstrap, or RAM.  BOOT0 is hardwired but BOOT1 can be used as a GPIO (with some restrictions) after the reset completes.  That's why you usually see external pull up/down resistors on the BOOT lines.

The STM32 datasheets go into detail on how BOOT pins work.

  Jack Peacock

waldin80
waldin80Author
Associate III
May 17, 2011
Posted on May 17, 2011 at 14:00

Thks for the help dudes, take care 0690X0000060MlGQAU.gif