Skip to main content
WGao.1
Associate II
Nov 29, 2020 3:51 PM UTC
Question

Function of ALERT pin(#19) for STUSB4500

In STUSB4500 datasheet, it says below for ALERT pin:

Pin 19, B2, ALERT, OD, I2C interrupt, active low open drain, To I2C master, ext. pull-up.

What does it mean - is the signal triggered when I2C command is sent from I2C master to STUSB4500?

Thanks,

Winston

This topic has been closed for replies.

5 replies

Peter BENSCH
ST Technical Moderator
Dec 2, 2020 1:10 PM UTC

ALERT is a signal from the STUSB4500 to the master and signals some transmission. You will also find it in the libraries, e.g. STSW-STUSB003. 

When your question is answered, please close this topic by choosing Select as Best.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
WGao.1
WGao.1Author
Associate II
Dec 2, 2020 10:32 PM UTC

Hi Peter,

Thanks for the answer. I have read the STW-STUSB003 but it does not give a hint as to when the signal will be sent.

That is what I want to know: can you give me some examples as to what transmission is signaled? Will the signal be sent once for each I2C transaction?

Thanks,

Winston

ST Employee
Dec 3, 2020 2:23 PM UTC

Hi Winston,

ALERT pin is not triggered I2C events but functional events. In the STSW-STUSB003 package, you can find a DOC directory which contains the product register map. ALERT pin behaviour can be configured by masking/unmasking relevant events or interrupts according to your application requirements. See ALERT_STATUS registers and similar @ 0x0B, 0x0C etc...

Hope it helps,

Rgds,

Benoit

FColl.1
Associate III
Apr 7, 2022 11:22 PM UTC

@Benoit FORET​  Why has the datasheet not been updated to include the functional description this pin?

ST Employee
Apr 14, 2022 2:54 PM UTC

Hi. Thanks for your suggestion.

So far, this is a choice we made to document software related features in a separate section.

Rgds