Skip to main content
Associate II
May 20, 2026
Solved

Function AFERead16BitBuffer() function in afe_config.c does not return a status

I am running the Analog Devices EVAL-ADE9430 board and noticed if I enable CRC checking reading 32 bit registers fail while 16-bit registers always pass.

I trace it down to the  AFERead16BitBuffer() function not returning a status after reading the register over the SPI bus. This allows 16 bit register reads to work all the time while 32 Bit registers fail all the time (that's another story).  

See line 12 below:     HAL_SPI_Receive(&hSPI, (uint8_t *)&pData[0], 2 * numSamples, SPI_TIMEOUT);

uint32_t AFERead16BitBuffer(uint16_t addr, uint16_t numSamples, uint16_t *pData)
{
 int32_t status = SYS_STATUS_SUCCESS;

 cmdBuffer[0] = (addr >> 4);
 cmdBuffer[1] = ((addr & 0x0F) << 4) + 8;

 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
 status = HAL_SPI_Transmit(&hSPI, (uint8_t *)&cmdBuffer, 2, SPI_TIMEOUT);
 if (status == 0)
 {
 HAL_SPI_Receive(&hSPI, (uint8_t *)&pData[0], 2 * numSamples, 
 SPI_TIMEOUT);
 }
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);

 SwapEndian16Bit(&pData[0], numSamples);

 DEBUG_MSG("REG16RD,0x%x,0x%x", addr, pData[0]);

 return status;
}

Compare this to the uint32_t AFERead32BitBuffer(), line 17 below which returns a status. 

uint32_t AFERead32BitBuffer(uint16_t addr, uint16_t numSamples, uint32_t *pData)
{
 int32_t status = SYS_STATUS_SUCCESS;

 cmdBuffer[0] = (addr >> 4);
 cmdBuffer[1] = ((addr & 0x0F) << 4) + 8;

 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_RESET);
 status = HAL_SPI_Transmit(&hSPI, (uint8_t *)&cmdBuffer, 2, SPI_TIMEOUT);
 /* FIXME : Handling SPI_Transmit error*/
 if (status != 0)
 {
 status = HAL_SPI_Transmit(&hSPI, (uint8_t *)&cmdBuffer, 2, SPI_TIMEOUT);
 }
 if (status == 0)
 {
 status = HAL_SPI_Receive(&hSPI, (uint8_t *)&pData[0], 4 * numSamples,
 SPI_TIMEOUT);
 }
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
 SwapEndian32Bit(&pData[0], numSamples);

 DEBUG_MSG("REG32RD,0x%x,0x%x", addr, pData[0]);

 return status;
}

Thanks - mike



Amy323Best answer
Visitor II
May 20, 2026

In AFERead16BitBuffer(), it looks like the receive result is getting ignored. You set status from HAL_SPI_Transmit(), but HAL_SPI_Receive() runs without assigning its return value back to status.

So this line:

HAL_SPI_Receive(&hSPI, (uint8_t *)&pData[0], 2 * numSamples, SPI_TIMEOUT);

could probably be:

status = HAL_SPI_Receive(&hSPI, (uint8_t *)&pData[0], 2 * numSamples, SPI_TIMEOUT);

That would make the function report a receive failure properly, same as the 32-bit version. Also worth being careful with the endian swap and debug print after a failed receive, since the buffer may not contain valid data in that case.

Pavel’s point about CRC is worth checking too, but the missing status assignment in the 16-bit path does look like a real bug either way.

7 replies

Pavel A.
May 20, 2026

Are you sure that the CRC algo of the STM32 SPI matches the CRC algo of the AD device? Would it be better to do the CRC in software?

 

 

mike_mAuthor
Associate II
May 21, 2026

Hi Pavel,

Thanks, the CRC does not match but that is not what the problem is. The problem is the AFERead16Bitbuffere() function is never returning a status.  

Best Regards - mike

Amy323Best answer
Visitor II
May 20, 2026

In AFERead16BitBuffer(), it looks like the receive result is getting ignored. You set status from HAL_SPI_Transmit(), but HAL_SPI_Receive() runs without assigning its return value back to status.

So this line:

HAL_SPI_Receive(&hSPI, (uint8_t *)&pData[0], 2 * numSamples, SPI_TIMEOUT);

could probably be:

status = HAL_SPI_Receive(&hSPI, (uint8_t *)&pData[0], 2 * numSamples, SPI_TIMEOUT);

That would make the function report a receive failure properly, same as the 32-bit version. Also worth being careful with the endian swap and debug print after a failed receive, since the buffer may not contain valid data in that case.

Pavel’s point about CRC is worth checking too, but the missing status assignment in the 16-bit path does look like a real bug either way.

mike_mAuthor
Associate II
May 21, 2026

Hi Amy323,

Thanks, the CRC does not match but as you know I am writing about the bug in the code where the AFERead16Bitbuffere() function is never returning a status. Hopefully this is the proper place to write about bugs? 

Best Regards - mike

ST Technical Moderator
May 21, 2026

Hello @mike_m 

What happens during step-by-step execution of the code? Does it stop at a particular instruction?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om