Skip to main content
Associate III
Apr 4, 2025 5:10 AM UTC
Solved

FreeRTOS SYSTickTimer frequency

Hi

I am trying to run freeRTOS on STM32f407 so I want to know at what frequency my clock will run let me share you my clocking diagram too.

another doubt how to enable SysTick_Handler.

other external interrupt I have enabled like this 

NVIC_SetPriority(TIM2_IRQn, 0x00);

NVIC_EnableIRQ(TIM2_IRQn);

NVIC_SetVector(TIM2_IRQn, (uint32_t)&TIM2_IRQ_Handler);

Note :

#define configSYSTICK_CLOCK_HZ ( configCPU_CLOCK_HZ )
#define configCPU_CLOCK_HZ ( ( unsigned long ) 16000000 )

is it correct

B.R

Ashish

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 4, 2025 11:09 AM UTC

Hello,

First , please use CubeMX to generate a FreeRTOS project. 

Second, in CubeMx, FreeRTOS needs system tick not a timer for its kernel tick. Need to select another timer for HAL:

Example TIM6:

mALLEm_0-1743764474608.png

Third, the system tick FreeRTOS kernel is running at 1ms rate: 

From FreeRTOSConfig.h:

#define configTICK_RATE_HZ ( ( TickType_t ) 1000 )

Attached an ioc file.

Hope that helps.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

6 replies

mƎALLEm
ST Technical Moderator
Apr 4, 2025 7:30 AM UTC

Hello, 

Please use </> button to share your code.

Thank you 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Ash1Author
Associate III
Apr 4, 2025 7:54 AM UTC

hi 

I cant share you code sorry to say but if you need more data you can ask in reply.

B.R

Ashish

Andrew Neil
Super User
Apr 4, 2025 8:24 AM UTC

What @mƎALLEm means is that you need to use the proper formatting for the code that you did include in your post.

See How to insert source code for full instructions.

See also How to write your question to maximize your chances to find a solution.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.