Skip to main content
Associate II
Sep 19, 2025 8:41 AM UTC
Solved

FreeRTOS PROBLEM

Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.

in STM32U073MCT6 microcontrollers, I have a problem which is like this;
in main.c I have

while (1)
{
 /* USER CODE END WHILE */
 HAL_GPIO_WritePin(ioOUT_DISP_A_GPIO_Port, ioOUT_DISP_A_Pin, 1);
 /* USER CODE BEGIN 3 */
}


and my led is blinked which is high 3.3 v
however, whenever I enable freertos, led is 0 v
what should I do?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 19, 2025 8:51 AM UTC

Hello,

As soon as osKernelStart() is called that infinite loop in main() is unreachable.

You need to handle that gpio state in one of the Tasks, example the default task.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

2 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 19, 2025 8:51 AM UTC

Hello,

As soon as osKernelStart() is called that infinite loop in main() is unreachable.

You need to handle that gpio state in one of the Tasks, example the default task.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
ST Technical Moderator
Sep 19, 2025 10:53 AM UTC

Hello @JamesMoriarty 

As @mƎALLEm mentioned you need to toggle your led in one of the tasks. 

Please check the example below as reference.

STM32CubeH7/Projects/NUCLEO-H743ZI/Applications/FreeRTOS/FreeRTOS_ThreadCreation at master · STMicroelectronics/STM32CubeH7 · GitHub 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om