FreeRTOS Dynamic Memory Management (STM32F4)
- 2 replies
- 2737 views
Please see attachment .pdf to see the content I excluded for brevity.
I have a project with various communication stacks. Messages arrive through one port, and may be processed locally, or routed to another port. Additionally messages may be generated locally and sent to a port. These messages vary significantly in size, with most being less than 64 bytes, but occasionally there will be a packet approaching 1024 Bytes. However, the sizes may be any ware from 1 to 1024 bytes.I am trying to understand if FreeRTOS supports a fragmentation-safe feature for passing these variable-length packets between threads and between ISR and thread. For example, is it possible to use malloc() in conjunction with Message Queues (with the producer passing a reference to the allocated memory) without fragmentation concern.
I see in the Heap_4.c source code that it, �combines (coalescences) adjacent memory blocks as they are freed, and in so doing limits memory fragmentation.� However, this still concerns me because my product may not be reset for months of run-time. It seems very difficult to test if the coalescence scheme is effective enough.
I was considering the scheme described here �
http://www.barrgroup.com/Embedded-Systems/How-To/Malloc-Free-Dynamic-Memory-Allocation
� which I�ll paste below:
[See attachment For this content]
I�ve read the �Memory Management� documentation of FreeRTOS �
http://www.freertos.org/a00111.html
� as well as skimmed the source code, but I am not confident that the heap implementation will meet my requirements.
I will paste �Memory Management� documentation below as well.
[See attachment For this content]
Questions:
1)
Am I correct in my assessment that that the FreeRTOS heap implementation is not fragmentation-safe?
� and if yes �
2)
Is there a �typical/canned solution� for this issue that can be implemented �on top� of FreeRTOS/CMSIS? E.g. the Memory Pool scheme.
See also:
http://asf.atmel.com/docs/latest/uc3b/html/group__membag__group.html
#freertos-heap-malloc-fragmentati