Skip to main content
JDWBE
Associate III
Apr 6, 2025 4:30 PM UTC
Question

Free-RTOS and mDNS

Hello Community!

I'm busy with a project that needs support for mDNS, after a long search i can't find any documentation howto implement mDNS on a Free-RTOS system. The examples provided by ST are not aware of any OS (I Think).

Can someone share some information please?

This topic has been closed for replies.

4 replies

Pavel A.
Apr 6, 2025 8:40 PM UTC

Here: https://www.freertos.org/Documentation/03-Libraries/02-FreeRTOS-plus/02-FreeRTOS-plus-TCP/02-Networking-basics/21-mDNS

FreeRTOS+ TCP supports mDNS. Why you prefer LwIP over FreeRTOS+ TCP?

LwIP does support mDNS as well:  https://www.nongnu.org/lwip/2_1_x/group__mdns.html

 

JDWBE
JDWBEAuthor
Associate III
Apr 7, 2025 10:53 AM UTC

Hello

 

Many thanks for your post.

When m i add this line in this way (right after lwip init, i use static ip):

 static void srv_txt(struct mdns_service *service, void *txt_userdata)
 {
 res = mdns_resp_add_service_txtitem(service, "path=/", 6);
 LWIP_ERROR("mdns add service txt failed\n", (res == ERR_OK), return);
 }

//Inside Default Thread
....
// Init LWIP

LOCK_TCPIP_CORE();
mdns_resp_add_service(&gnetif, "myweb", "_http", DNSSD_PROTO_TCP, 80, 3600, srv_txt, NULL);
UNLOCK_TCPIP_CORE();

I Get this error on the terminal (When running):

Assertion "mdns_resp_add_service: Not an mdns netif" failed at line 2202 ... Middlewares/Third_Party/LwIP/src/apps/mdns/mdns.c

Maybe i forgot something to enable or i understand the implementation wrong?

 

I got exactly one ping back from the board, then it is dead. When i remove the mDNS stuff, the board works fine.

JDWBE
JDWBEAuthor
Associate III
Apr 10, 2025 8:42 AM UTC

Hello

Is there any suggestion what i can try?

Kind Regards

Pavel A.
Apr 10, 2025 8:48 AM UTC

Try to debug, sometimes it helps. Questions about LwIP and its applications can be also asked on Stack Overflow.