Skip to main content
MK..1
Associate III
Jun 6, 2024 9:32 AM UTC
Solved

FP-SNS-ALLMEMS1 not found in cube ide

Hi

I am trying to set up a project based on FP-SNS-ALLMEMS1.

When i set up a project based on STM32L476 Nucleo, I cant find the pack neither under "select components" nor under "manage software packs". see below

Why??

MK1_0-1717666159417.png

 

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jun 6, 2024 2:48 PM UTC

Unfortunately, not all software packages are yet integrated in STM32CubeIDE, so that in such cases it is only possible to open or create projects manually. To do this, you can download the firmware FP-SNS-ALLMEMS1, unpack it (for Windows, please use short paths) and open the STM32L476RG-Nucleo projects directly from there, for example.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jun 6, 2024 2:48 PM UTC

Unfortunately, not all software packages are yet integrated in STM32CubeIDE, so that in such cases it is only possible to open or create projects manually. To do this, you can download the firmware FP-SNS-ALLMEMS1, unpack it (for Windows, please use short paths) and open the STM32L476RG-Nucleo projects directly from there, for example.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.