Skip to main content
Visitor II
Jan 30, 2025 1:45 PM UTC
Question

FMC gives no output for LCD

Hello,

Apologies if this is posted in the wrong location. I am trying to control an LCD (ST7789) with my STM32U5G9J-DK2 using FMC. In CubeMX, I configured the NOR Flash/PSRAM/SRAM/ROM/LCD 1 to use NE1 and A0 with 16 bits of data. I also ensured to configure the NOR/PSRAM timing according to the ST7789 datasheet.

To my limited understanding of FMC, I believe that writing to the memory bank I have FMC set up at will cause the STM to automatically handle my control signals (FMC_A0, FMC_NE1, FMC_NWE, FMC_NOE, and data). Because I am using NE1 and A0, I have my memory locations defined as:

 

 

#define FMC_BANK1_REG ((uint32_t *)0x60000000)
#define FMC_BANK1_DATA ((uint32_t *)0x60000002)

 

 

 And I am using the functions below to read and write:

 

 

void write_command(uint8_t data)
{
 *FMC_BANK1_REG = (uint32_t)data;
}

void write_data(uint8_t data)
{
 *FMC_BANK1_DATA = (uint32_t)data;
}

uint16_t read_data() {
	return *FMC_BANK1_DATA;
}

// Example
write_command(0xFF);
write_data(0xFF);
HAL_Delay(1000);
uint16_t d = read_data();

 

 

I am using the CubeMX generated code for initialization. After initialization, I try to write some data, and I then try to read it back. However, the data is always 0 for some reason. Why is this?

This topic has been closed for replies.

1 reply

ST Technical Moderator
Jan 30, 2025 6:54 PM UTC

Hello @user20324-245 ,

Check the timing parameters in CubeMX and ensure they match the requirements of the ST7789 datasheet. Incorrect timing settings can lead to improper communication with the LCD.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks