Skip to main content
Associate
Aug 6, 2025 12:05 AM UTC
Solved

Flash write fails when using mcumgr from zephyr to upload an image

I'm using the nucleo-H753ZI board to test mcuboot.

The setup works and I can successfully run the bootloader and the application in slot0_partition using zephyr sysbuild.
However when trying to upload an image I get the following flash write error:

[00:00:29.758,000] <inf> mcuboot_util: Image index: 0, Swap type: none
[00:00:29.758,000] <inf> mcuboot_util: Image index: 0, Swap type: none
[00:00:29.922,000] <err> flash_stm32h7: Status Bank2: 0x00040000
[00:00:29.922,000] <err> STREAM_FLASH: flash_write error -5 offset=0x00100000
[00:00:29.922,000] <err> mcumgr_img_grp: Irrecoverable error: flash write failed: 12

Here is my flash0 dts:

&flash0 {
partitions {
compatible = "fixed-partitions";
#address-cells = <1>;
#size-cells = <1>;

boot_partition: partition@0 {
label = "mcuboot";
reg = <0x00000000 DT_SIZE_K(128)>;
};
slot0_partition: partition@20000 {
label = "image-0";
reg = <0x00020000 DT_SIZE_K(896)>;
};
slot1_partition: partition@100000 {
label = "image-1";
reg = <0x00100000 DT_SIZE_K(896)>;
};
storage_partition: partition@1e0000 {
label = "storage";
reg = <0x001e0000 DT_SIZE_K(128)>;
};
};
};

I have also attached the .config file from the build output as reference.

Appreciate any help to get this resolved. I assume it is some KCONFIG settings which is causing this.
This topic has been closed for replies.
raphaZahndBest answer
Associate
Sep 12, 2025 2:15 PM UTC

Turns out it was a stm32_flash driver bug in the zephyr repo recently fixed: https://github.com/zephyrproject-rtos/zephyr/commit/ea1245eb92000d3fe24d2b974754714973ce5ab1 Works with this fix also when slot2 is in bank2!

3 replies

Associate
Aug 15, 2025 10:20 PM UTC

Unfortunately I'm still stuck with the flash write error during a application image upload with mcumgr. Any help would be appreciated. Thanks!

Associate
Sep 12, 2025 8:17 AM UTC

Having both slots in bank1 fixes the issue and I can successfully upgrade the firmware with the mcumgr and there is NO flash write error: [00:00:29.922,000] <err> flash_stm32h7: Status Bank2: 0x00040000 (PGSERR).

However that let's me waste the other 1MB of flash in bank2. So still unclear why writing into bank2 doesn't work while writing into bank1 works.

raphaZahndAuthorBest answer
Associate
Sep 12, 2025 2:15 PM UTC

Turns out it was a stm32_flash driver bug in the zephyr repo recently fixed: https://github.com/zephyrproject-rtos/zephyr/commit/ea1245eb92000d3fe24d2b974754714973ce5ab1 Works with this fix also when slot2 is in bank2!