Skip to main content
Associate II
Mar 5, 2026 7:18 AM UTC
Question

Flash Memory programming for STM32F407

Hello Everyone,

This is the code that I have tried many times and tried to debug as well. I have attached a snapshot of the error of the debugging section (disassembly ). I have not been able to understand what of my code leads to this error , and how to solve this?

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2026 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "string.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define FLASHSTART_SECTOR_11 0x080E0000
#define OB_START 0x1FFFC000
#define FI_START 0x40023C00 //flash interface register start address
#define FLASH_CR (*((volatile uint32_t *)0x40023C10))
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart1;

/* USER CODE BEGIN PV */

uint32_t data2[10] = {1,2,3,4,5,6,7,8,9};
uint32_t Rx_Data[30];

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
/* USER CODE BEGIN PFP */

uint32_t Flash_Write_Data (uint32_t StartSectorAddress, uint32_t *Data, uint16_t numberofwords);
void Flash_Read_Data (uint32_t StartSectorAddress, uint32_t *RxBuf, uint16_t numberofwords);

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART1_UART_Init();
 /* USER CODE BEGIN 2 */
 // Write_flash();
 Flash_Write_Data(0x080E0000 , data2, 9);
 Flash_Read_Data(0x080E0000 , Rx_Data, 10);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 HAL_UART_Transmit(&huart1,(const uint8_t *)Rx_Data, 36, 100);
	 HAL_Delay(1000);


 }
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */

 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 168;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief USART1 Initialization Function
 * None
 * @retval None
 */
static void MX_USART1_UART_Init(void)
{

 /* USER CODE BEGIN USART1_Init 0 */

 /* USER CODE END USART1_Init 0 */

 /* USER CODE BEGIN USART1_Init 1 */

 /* USER CODE END USART1_Init 1 */
 huart1.Instance = USART1;
 huart1.Init.BaudRate = 115200;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART1_Init 2 */

 /* USER CODE END USART1_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

uint32_t Flash_Write_Data (uint32_t StartSectorAddress, uint32_t *Data, uint16_t numberofwords)
{

	static FLASH_EraseInitTypeDef EraseInitStruct;
	uint32_t SECTORError;
	int sofar=0;


	 /* Unlock the Flash to enable the flash control register access *************/
	 HAL_FLASH_Unlock();

	 FLASH_CR &= ~(0x3U << 8);
	 FLASH_CR |= (0x2U << 8);
	 /* Erase the user Flash area */


	 /* Fill EraseInit structure*/
	 EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
	 EraseInitStruct.VoltageRange = FLASH_VOLTAGE_RANGE_3;
	 EraseInitStruct.Sector = FLASHSTART_SECTOR_11;
	 EraseInitStruct.NbSectors = 1;

	 /* Note: If an erase operation in Flash memory also concerns data in the data or instruction cache,
	 you have to make sure that these data are rewritten before they are accessed during code
	 execution. If this cannot be done safely, it is recommended to flush the caches by setting the
	 DCRST and ICRST bits in the FLASH_CR register. */

	 __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR );//obligatorily...

	 if (HAL_FLASHEx_Erase(&EraseInitStruct, &SECTORError) != HAL_OK)
	 {
		 return HAL_FLASH_GetError ();
	 }

	 /* Program the user Flash area word by word
	 (area defined by FLASH_USER_START_ADDR and FLASH_USER_END_ADDR) ***********/

	 while (sofar<numberofwords)
	 {
	 if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, StartSectorAddress, Data[sofar]) == HAL_OK)
	 {
	 	 StartSectorAddress += 4; // use StartPageAddress += 2 for half word and 8 for double word
	 	 sofar++;
	 }
	 else
	 {
	 /* Error occurred while writing data in Flash memory*/
	 	 return HAL_FLASH_GetError ();
	 }
	 }

	 /* Lock the Flash to disable the flash control register access (recommended
	 to protect the FLASH memory against possible unwanted operation) *********/
	 HAL_FLASH_Lock();

	 return 0;
}

void Flash_Read_Data (uint32_t StartSectorAddress, uint32_t *RxBuf, uint16_t numberofwords)
{
	while (1)
	{
		*RxBuf = *(__IO uint32_t *)StartSectorAddress;
		StartSectorAddress += 4;
		RxBuf++;
		if (!(numberofwords--)) break;
	}
}
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

Initially I tried the code without 
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR );


, that was when I was only to able to program the board once. After that it used to give some error 
Error: ST-LINK error (DEV_TARGET_NOT_HALTED).

 

I want to save some data in the flash so that I can use that after powering the board again. The data is of float

data-type and 12 such floats have to be saved. Is there any way I can tackle this issue?

The code is in reference with this:click here.

 
 
 

Screenshot 2026-03-05 123759.png

3 replies

TDK
Mar 5, 2026 1:46 PM UTC

Writing to flash at the start of the program will not let the debugger connect. Put a HAL_Delay(500) before doing any flash operations.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
SohamCAuthor
Associate II
Mar 6, 2026 10:03 AM UTC

Okay , I will try to put hal_delay() at the start.
It would be great if you could explain what the error was , of which a snapshot is attached. And are there any things that I should keep in mind while writing the final version of the firmware.