Skip to main content
Associate
Mar 19, 2026 10:35 AM UTC
Solved

FLASH_EraseProgram example code for STM32CubeU3 not working. fails in erasing

I am running the  FLASH_EraseProgram example code provided by STM32CubeU3.  the code fails in erasing the flash and enters ErrorHandler.

 

I have verified the FLASH_USER_START_ADDR & FLASH_USER_END_ADDR.  it is set as follows. 

#define FLASH_USER_START_ADDR ADDR_FLASH_PAGE_128 /* Start @ of user Flash area */
#define FLASH_USER_END_ADDR (ADDR_FLASH_PAGE_255 + FLASH_PAGE_SIZE - 1) /* End @ of user Flash area */

I have tested in both debug and run mode, it is not working as expected. Is anything to be modified to run the code.

 

regards,

Rajath

 

rajathksBest answer
Associate
Mar 19, 2026 1:23 PM UTC

Hi TDK,

I resolved the issue. I reset the option bytes to default factory settings.  I think the wrong bank was selected in option byte.

Also observed setting breakpoint in code is affecting the flash erase operation.

 

Thanks for the help!!

regards,

Rajath 

 

4 replies

TDK
Mar 19, 2026 12:48 PM UTC

FLASH_EraseProgram should not be called directly. Use HAL_FLASHEx_Erase as is done in the example programs like this one:

https://github.com/STMicroelectronics/STM32CubeU3/blob/453c7fafaeb4774b4b0f6e4f8486e7c183fc254e/Projects/NUCLEO-U3C5ZI-Q/Examples/FLASH/FLASH_EraseProgram/Src/main.c#L146

Show your code.

"If you feel a post has answered your question, please click ""Accept as Solution""."
rajathksAuthor
Associate
Mar 19, 2026 12:58 PM UTC

Hi TDK,

I am using  the following example code in STM32CubeU3 without any changes. 

Projects/NUCLEO-U385RG-Q/Examples/FLASH/FLASH_EraseProgram

The program does not work properly, Flash page erase fails with PGSERR .

regards.

Rajath

TDK
Mar 19, 2026 1:10 PM UTC

No such issues here running it in STM32CubeIDE. Are you loading it with the Example Selector in STM32CubeMX?

"If you feel a post has answered your question, please click ""Accept as Solution""."
rajathksAuthorBest answer
Associate
Mar 19, 2026 1:23 PM UTC

Hi TDK,

I resolved the issue. I reset the option bytes to default factory settings.  I think the wrong bank was selected in option byte.

Also observed setting breakpoint in code is affecting the flash erase operation.

 

Thanks for the help!!

regards,

Rajath