Skip to main content
RVelh.345
Explorer
Jun 1, 2020 10:09 AM UTC
Question

Firmware update via CAN bootloader with multiple nodes in bus

Hello,

I'm working with the stm32f439ZG and I have one question regarding the CAN bootloader.

I'm trying to update one node via CAN interface.

I have one network with 3 nodes (the node 1 is responsible for send the new firmware, the node 2 will receive this new firmware and the node 3 is idle). My "normal" CAN bitrate is 500kbits.

My strategy is:

1. node 1 sends one message that forces nodes to stop sending messages;

2. node 1 sends one message that forces node 2 to enter in bootloader and node 3 execute the function HAL_CAN_DeInit(&hcan2) and after MX_CAN2_Init_125(), init CAN with CAN bitrate=125kbits;

3. node 3 has one CAN filter that blocks all the Standard IDs.

However, when I send the sync message (0x79) the node 2 jumps off the bootloader.

What is the right approach for execute the firmware update via CAN when have in the network multiple nodes?

Thanks for your help.

This topic has been closed for replies.

1 reply

Associate
Jul 27, 2024 8:53 AM UTC

hi, did you find solution?