Skip to main content
42bytes
Visitor II
Oct 28, 2022 10:42 AM UTC
Question

Firmware update over uart I/O pin config

Hello together

Actual I use the systembootloader to update the device over uart.

Is there a way to reconfigure the unused I/O pin for the system bootloader? Or must this be done via a self-written bootloader?

The problem is that some I/O pins take on a different status as soon as the application for the firmware update jumps into the system bootloader.

Thank you and br

This topic has been closed for replies.

1 reply

MM..1
Super User
Oct 28, 2022 2:18 PM UTC

Systembootloader can be used only with pins defined in AN2606