Skip to main content
This topic has been closed for replies.
nicolas
nicolasBest answer
Senior II
Jun 17, 2025 7:21 AM UTC

My current solution is to copy the folder FileX\ports\cortex_m3 into FileX\ports\cortex_m33 but i'm not satisfied with it because i need to manually copy this folder or to fork the stm32-mw-filex repo. It would be best to have the stm32-mw-filex repo support m33 so I have open an issue.

7 replies

ST Technical Moderator
Jun 13, 2025 1:09 PM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
nicolas
nicolasAuthor
Senior II
Jun 13, 2025 3:09 PM UTC

Thanks for the answer.

But this example doesn't use CMake, and it also doesn't use ThreadX.

Without ThreadX, i think i could build FileX with THREADX_ARCH = generic.

ST Technical Moderator
Jun 13, 2025 3:50 PM UTC

Hello @nicolas 

You can use the existing IOC file, then add THREADX and generate cmake project. 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om