Skip to main content
PB S.1
Associate II
May 26, 2023 11:18 AM UTC
Solved

File System to store HTML Web pages in NUCLEO-H745-ZIQ

I am trying to develop simple HTTP Web Server using NUCLEO-H745-ZIQ board.

The idea is to have file system to store our HTML web pages.

Do you have an example code to achieve this ? Or else please suggest us a way to have file system to load our html pages using NUCLEO-H745-ZIQ board.

This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
May 31, 2023 3:36 PM UTC

Hi @PB S.1​,

  1. You can find the file system under this link. Projects/STM32H743I-EVAL/Applications/LwIP/LwIP_HTTP_Server_Raw/Fs
  2. To use FS data file, you can refer to HTTPD_FSDATA_FILE in httpd_opts.h. Then, you can specify FS_ROOT and add the appropriate entry for your custom HTML file.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

7 replies

Nikita91
Lead II
May 26, 2023 2:28 PM UTC
ST Technical Moderator
May 30, 2023 5:26 PM UTC

Hello @PB S.1​,

You can migrate the following example used for NUCLEO-H743 under Projects\NUCLEO-H743ZI\Applications\LwIP 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
PB S.1
PB S.1Author
Associate II
May 31, 2023 7:18 AM UTC

Hi @F.Belaid​ ,

I found an example project under the repository that you have mentioned.

I wanted to know how to generate fsdata_custom.c.

Suppose if I want to add my HTML web files, how to generate fsdata_custom.c corresponding to my web files?

ST Technical Moderator
May 31, 2023 8:17 AM UTC

Hello again @PB S.1​,

To include "fsdata_custom.c" instead of "fsdata.c" for the file system (to prevent changing the file included in CVS) you should set this to 1.

#define HTTPD_USE_CUSTOM_FSDATA  1 

 You can find this define in lwipopts.h.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL