Skip to main content
Karthik Kumar
Associate II
Aug 30, 2022 6:23 AM UTC
Question

FDCAN Receive data issue in STM32G0B1RE

Hello Every One!!

I am Using NUCLEO G0B1RE Board, facing Issue with CAN Receive Function I am using MICROCHIP CAN BUS ANALYSER and NUCLEO BOARD for CAN Communication

void CAN_Recieve(void){

while( (HAL_FDCAN_GetRxFifoFillLevel(&hfdcan1,FDCAN_RX_FIFO0)   < 1  )  )

{

}

if(HAL_FDCAN_GetRxMessage(&hfdcan1,FDCAN_RX_FIFO0, &RxHeader ,RxData) != HAL_OK)

{

  Error_Handler();

 }

}

and also in my main function after all the HAL inits for my project

while(1)

{

CAN_Recieve();

ADC_Calculation();

delay_ms(1000); //1sec

PWM_Control();

 }

let me explain what i have observed

for the first time when i send data from CANALYSER to Nucleo Board it receives Identifier and Data sucessfully, If i dont send the CAN message from CANALYSER for the send time the MCU is hang in the While Loop ,its not executing ADC calculation and PWM_Control functions in my main function

this is the API

while( (HAL_FDCAN_GetRxFifoFillLevel(&hfdcan1,FDCAN_RX_FIFO0)   < 1  )  )

{

}

unless until I send another CAN message from CANALYSER it reads sucessfully.

I want to resume my Main Function even if send the CAN message from CANALYSER or not it should execute my Main function while Loop

please suggest me

Regards,

Karthik

This topic has been closed for replies.