Skip to main content
Associate II
Feb 19, 2025 9:17 AM UTC
Question

FatFs_uSD_Standalone Example for STM32G474E_EVAL board

Hello,

I'm new to this community  and I'm trying to learn from different examples that are available online. I have STM32G474E-EVAL1 board and I want to include the sd card in one of my projects. So I founded the FatFs_uSD_Standalone Example that was originally for the STM32G474E-EVAL board. I was able to compile it successfully and tried to run it in the debug mode on my EVAL1 board but it fails in the 'SD_GoIdleState(void)' function. Is there any particular reason that the code wouldn't run properly on my EVAL1 board ? I've checked that the sd connector does receive 3.3 V.

Thanks in advance

 

This topic has been closed for replies.

6 replies

ELABI.1
ST Technical Moderator
Feb 19, 2025 2:14 PM UTC

Hi @Ana ,

In fact, the STM32G474E-EVAL1 is recommended to be used for the motor control configuration board

This information is already mentioned below:

ELABI1_0-1739974460258.png

When comparing the obsolete STM32G474E-EVAL Board REV B-04 with the STM32G474E-EVAL1 board, we found that the uSD chip select pin does not fit. Therefore, the uSD chip select pin (PF8) must be fitted on the STM32G474E-EVAL1 Board.

ELABI1_1-1739978706379.jpeg

 

Thank you.

ELABI.1

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AnaAuthor
Associate II
Mar 9, 2025 11:45 AM UTC

Hi,

In addition to your previous answer, On the obsolete STM32G474E-EVAL Board REV B-04 uSD CS pin is fitted and there is resistor R135 in place, how do I know what kind of a resistor I need to choose in order to make the uSD chip select pin (PF8) fitted on the STM32G474E-EVAL1 board ?

 

Thank you

AScha.3
Super User
Mar 9, 2025 5:34 PM UTC

Hi,

>how do I know what kind of a resistor -

as you can see in the -eval circuit, its 0R = NULL ohm. So use solder or a small piece of wire...thats it.

If you feel a post has answered your question, please click on " Best Answer ".
Andrew Neil
Super User
Feb 19, 2025 2:24 PM UTC

@Ana wrote:

Is there any particular reason that the code wouldn't run properly on my EVAL1 board ?


Check the schematics - are all the IOs required by the example free & available on the EVAL1 board ?

 


@Ana wrote:

I've checked that the sd connector does receive 3.3 V.


and what about all the other pins used by the SD-Card?

 


@Ana wrote:

it fails in the 'SD_GoIdleState(void)' function.


What debugging have you done to find how & why it "fails" ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
AnaAuthor
Associate II
Feb 20, 2025 10:02 AM UTC

Hi Andrew,

Thank you for the answer, I hope that the first reference will help to solve the problem. About your second reference - I have mistakenly checked the wrong board schematics, so I'll check again all the pins. About your third reference - I entered with the debugger into the hippest function and checked where and when exactly the ERROR CODE was updated, this actually happened when the SD card didn't return answer' so I suppose it's really more of a hardware problem.

I'll update here when I'll be able to fix the problem.

 

Thanks

AnaAuthor
Associate II
Feb 20, 2025 9:55 AM UTC

Hi,

Thank you so much for the reference, this board schematic is exactly what I was looking for (found on MXCube, the names of the files are a little bit confusing:

Image 20-02-2025 at 11.51.jpeg

Both of them are  B04 revisions and the part number in both of the files is the obsolete STM32G474E-EVAL.)

I'll update here if this helped to solve the problem.

Thank you