Skip to main content
Associate
Feb 25, 2025 11:04 AM UTC
Question

FATFS f_write error (9) when SAI/DMA is running

Hello, 

I am trying to record audio data from an ADC to a SD card with a nucleo STM32L552ZET6QU board. To write data into SD card using FatFs I initialised it  : 

"// Open the file system - mount the drive

fres = f_mount(&FatFs, "", 1); // 1 = mount now

if (fres != FR_OK) {

myprint("f_mount error (%i)\r\n", fres);

while(1);

}

// Statistics from the SD card

DWORD free_clusters, free_sectors, total_sectors;

FATFS* getFreeFs;

fres = f_getfree("", &free_clusters, &getFreeFs);

if (fres != FR_OK) {

myprint("f_getfree error (%i)\r\n", fres);

while(1);

}

//Formula comes from ChaN's documentation

total_sectors = (getFreeFs->n_fatent - 2) * getFreeFs->csize;

free_sectors = free_clusters * getFreeFs->csize;

myprint("SD card stats:\r\n%10lu KiB total drive space.\r\n%10lu KiB available.\r\n", total_sectors / 2, free_sectors / 2);

// Open file

fres = f_open(&fil, "record.bin", FA_WRITE | FA_CREATE_ALWAYS);

if(fres == FR_OK)

{

myprint("I was able to open 'record.bin' for writing\r\n");

}

else

{

myprint("f_open error (%i)\r\n", fres);

}

 

float data[4] = {1.2, 1.6, -0.5, 3.2};

UINT bytesWrote;

fres = f_write(&fil, data, sizeof(data), &bytesWrote);

if(fres == FR_OK)

{

myprint("Wrote %i bytes to 'record.bin'!\r\n", bytesWrote);

}

else

{

myprint("f_write error (%i)\r\n", fres);

}"

 

Everything goes fine, except when the SAI is enabled with I2S mode coupled with DMA1 and initialise with this line of code : 

"HAL_StatusTypeDef status = HAL_SAI_Receive_DMA(&hsai_BlockA1, (uint8_t *)adcData, BUFFER_SIZE*4);" 

After that, I only get "f_write error (9)" when I try to write into my file created before.

There must be a conflict between SAI/DMA and FATFS but I couldn't resolve it.

 

SD card is linked to SPI3 which is on APB1, SAI1 is on APB2 and DMA1 is on AHB1.

My SD card is formated in FAT32.

 

What could be the problem?

This topic has been closed for replies.

16 replies

ST Technical Moderator
Feb 27, 2025 10:45 AM UTC

Hello @JulesSTM32,

Could you please share your project so that we can support you more effectively?

Otherwise, could you try using polling mode for SAI and SPI? The source of the issue might be a bad management of interrupt priorities.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Associate
Feb 27, 2025 3:30 PM UTC

Hello, here is the link of my github repository : https://github.com/JulesAcwa/myproject_I2S_SAI_and_FATFS .

In theory, there is enough time to write my data in the SD card before another DMA interrupt happens. 

I don't use polling mode with the SAI in order to avoid data loss. The SPI is used under FATFS f_write function, which is equivalent to a polling mode isn't it ?  

Thank you for your reply. 

 

 

 

ST Technical Moderator
Feb 28, 2025 9:26 AM UTC

Hello @JulesSTM32 

Could you please check with different DMA interrupt priorities? I noticed that both channels are currently set with the same interrupt priorities.

Does the failure occur immediately upon starting execution, or does it happen after some time has passed?

Are you sure you have enough space on the uSD card?

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
AScha.3
Super User
Feb 28, 2025 9:40 AM UTC

Hi,

just - why dont you use SDMMC for sd-card ? L552 has a sdmmc interface , afaik.

I use SAI + SDMMC /sd-card for my audio player and there is no problem with them working same time.

If you feel a post has answered your question, please click on " Best Answer ".
Associate
Mar 3, 2025 10:22 AM UTC

Hi, I couldn't find a good tutorial using SDMMC interface for this specific application. Could you share your project with me so I can see your configuration and how you interact with the SD card ? 

ST Technical Moderator
Mar 4, 2025 8:42 AM UTC

Hello @JulesSTM32 

Please refer to these materials if you want to use SDMMC.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Associate
Mar 12, 2025 3:00 PM UTC

Hello,

I still have f_mount error (3). I double check de software configuration and I have no idea how to resolve it. However HAL_SD_GetCardStatus() works.

Thanks, 

Jules.

 

ST Technical Moderator
Mar 14, 2025 8:58 AM UTC

Hello @JulesSTM32 

Did you try to compare your config with the example Projects/STM32L552E-EV/Applications/FatFs/FatFs_uSD_DMA.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om