Skip to main content
Associate
Jun 16, 2025 1:28 PM UTC
Solved

F769 EVAL QSPI_Executeinplace example code

when running the QSPI_Executeinplace example code on the stm32f769i_eval board,the program enters HardFault_handler() after executing GpioToggle().i just remove the QSPI_DummyCyclesCfg(),in GpioToggle() the GPIO Not Taking effect,so How can I solve this problem?      thanks

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jun 16, 2025 2:58 PM UTC

Hello @andrewpei ,

Use a debugger to identify the exact instruction causing the HardFault.

Have you made any updates to the example?  If yes, please share the exact modifications you made and the debugger output when the HardFault occurs?

Ensure that the QSPI and GPIO peripherals do not have conflicting configurations or resource usage.

Ensure that the dummy cycles are correctly configured as per the QSPI memory datasheet.

Remember to use the latest release of CubeF7 firmware package.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

Imen.DBest answer
ST Technical Moderator
Jun 16, 2025 2:58 PM UTC

Hello @andrewpei ,

Use a debugger to identify the exact instruction causing the HardFault.

Have you made any updates to the example?  If yes, please share the exact modifications you made and the debugger output when the HardFault occurs?

Ensure that the QSPI and GPIO peripherals do not have conflicting configurations or resource usage.

Ensure that the dummy cycles are correctly configured as per the QSPI memory datasheet.

Remember to use the latest release of CubeF7 firmware package.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
andrewpeiAuthor
Associate
Jun 17, 2025 3:55 AM UTC

Hello,@Imen.D ,

Indeed, by debug the code, I found that the data written to NOR Flash differs from the original data,because the dummy cycle configuration for my NOR Flash under the QUAD_OUT_FAST_READ_CMD instruction differs from the example code's implementation. 

ST Technical Moderator
Jun 16, 2025 3:11 PM UTC

Hello @andrewpei 

Please refer to this article to debug hardfault.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om