Skip to main content
SSRIN.1
Associate III
Sep 21, 2021 5:30 AM UTC
Question

F767ZI+FreeRTOS+lwip can't support more than 2 clients?

I require to run 3 clients. I start 3 lwip threads using sys_thread_new. Each thread will service 3 python clients via 3 distinct Ports. Everything seems to be working when running only 2 threads . However, when a third client is added things become weird. Only one client is able to connect . When a second or third client tries to connect, it returns connection reset by peer.

This topic has been closed for replies.

5 replies

alister
Senior III
Sep 21, 2021 8:14 AM UTC

MEMP_NUM_TCP_PCB_LISTEN?

SSRIN.1
SSRIN.1Author
Associate III
Sep 21, 2021 8:36 AM UTC

Its marked as 8

alister
Senior III
Sep 21, 2021 8:58 AM UTC

HTTP/HTTPS?

LWIP_HTTPD_KILL_OLD_ON_CONNECTIONS_EXCEEDED?