Skip to main content
asttekin
Associate
Oct 20, 2025 3:15 PM UTC
Question

F103C8 USART DMA Issue

Hi,

I'm having the following issue with the F103C8 USART DMA.
After reset, sometimes the USART DMA Receive doesn't work. It doesn't happen every time, but it happens about once every 10 resets.

HAL_UARTEx_ReceiveToIdle_DMA(&huart1, (uint8_t *)RxDataUsart1, 128);
__HAL_DMA_DISABLE_IT(&hdma_usart1_rx, DMA_IT_HT);

HAL_UARTEx_ReceiveToIdle_DMA(&huart2, (uint8_t *)RxDataUsart2, 128);
__HAL_DMA_DISABLE_IT(&hdma_usart2_rx, DMA_IT_HT);
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
{
	if(huart == &huart1)
	{
		timer_UART1_Datalost = millis();
		uart_1_Ready	= SET;
		__HAL_UART_CLEAR_FEFLAG(&huart1);
		memcpy(copyRxDataUsart1, RxDataUsart1, 128);
		copyRxDataUsart1[127] = '\0';
		usart1Datareceived = 1;

		for (int i=Size; i < 128; i++)RxDataUsart1[i]=0;
	}
	__HAL_UART_ENABLE_IT(&huart1, UART_IT_IDLE);
	HAL_UARTEx_ReceiveToIdle_DMA(&huart1, (uint8_t *)RxDataUsart1, 128);
	__HAL_DMA_DISABLE_IT(&hdma_usart1_rx, DMA_IT_HT);

	if(huart == &huart2)
	{
		uart_2_Ready	= SET;
		__HAL_UART_CLEAR_FEFLAG(&huart2);
		memcpy(copyRxDataUsart2, RxDataUsart2, 128);
		copyRxDataUsart2[127] = '\0';
		usart2Datareceived = 1;
		for (int k=Size; k < 128; k++)RxDataUsart2[k]=0;
	}
	__HAL_UART_ENABLE_IT(&huart2, UART_IT_IDLE);
	HAL_UARTEx_ReceiveToIdle_DMA(&huart2, (uint8_t *)RxDataUsart2, 128);
	__HAL_DMA_DISABLE_IT(&hdma_usart2_rx, DMA_IT_HT);

}

 

This topic has been closed for replies.

3 replies

Andrew Neil
Super User
Oct 20, 2025 3:23 PM UTC

@asttekin wrote:

USART DMA Receive doesn't work


What, exactly, does that mean?

  • It receives nothing ?
  • It receives something - but incomplete ?
  • It receives something - but corrupt ?
  • Other ?
  • A combination of the above ?

 

Does it work reliably without DMA ?

 

Please show a minimum but complete example which illustrates the issue.

 

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
asttekin
asttekinAuthor
Associate
Oct 20, 2025 3:37 PM UTC

No action.
No data reception.
No data completion.

Does it work reliably without DMA?
I haven't tried it. 

AScha.3
Super User
Oct 20, 2025 8:52 PM UTC

Hi,

what speed you have on uart ?  many Mbit ?

or: why DMA here ? 

+

The problem here is probably : what you do, if a spike sets the uart to an error condition?

Without clearing the error, nothing happens - until you clear it.

Seems this is the "problem" here.

So include some useful error handling, or do it in INT mode, clearing an error, if it happens.

Then you get reliable uart communication.

If you feel a post has answered your question, please click on " Best Answer ".