Skip to main content
Associate III
April 23, 2026
Question

External QSPI NOR flash read and write operation

Hi, 

I’m working on a custom board based on STM32H757BITx using an external NOR flash Micron MT25TL01GBBB8ESF-0AAT TR (Dual bank with Quad Lines)

Current usage

At the moment, the external flash is mainly used to store UI assets (images/fonts/etc.) for a display. I’m not using the full flash capacity, so I’d like to use an unused region to store a small persistent structure (configuration/status/log header).

To keep things organized, I created a partitioning scheme using the linker file, reserving separate address ranges:

  • UI assets region (read-only at runtime)
  • User structure region (needs occasional write/erase/program)

How it’s configured right now

Since up to now I only needed runtime reads, the flash is configured in Memory-Mapped Mode (DTR, QPI). I enable it with:

MT25TL01G_EnableMemoryMappedModeDTR(&hqspi, MT25TL01G_QPI_MODE);
This works great for reading UI assets through the mapped address space.
 

Problem

I now need to write into the user structure region, but I understand that in Memory-Mapped Mode the peripheral is configured for read transactions and typical write/erase operations require switching back to indirect mode (command mode).

Questions

  1. Is it safe / supported to temporarily exit memory-mapped mode, perform:

    • sector erase (as needed)
    • page program for the structure and then re-enter memory-mapped mode (DTR/QPI) again?
  2. If yes, what is the recommended sequence on STM32H757 to exit memory-mapped mode cleanly?
    For example: abort memory-mapped, re-init, switch to indirect, do erase/program, then enable memory-mapped again.

  3. RTOS (ThreadX):
    Even though only the CPU reads the memory-mapped region (no LTDC/DMA2D direct reads from external flash), I have multiple threads. While one thread is writing to flash, another thread might try to read UI assets (mapped reads).

    • Is a mutex/semaphore around any access to the memory-mapped region the right approach?
  4. Cache coherency:
    When returning to memory-mapped mode after writing, do I need to do DCache clean/invalidate.

Please find attached the source files containing the functions that access/call the external flash.

 

If anyone has done something similar,  I’d love to hear best practices.
 
Thanks!

3 replies

Ayoub Cheggari
Senior
April 23, 2026

Hi,

I tried that once for HMI also and it didn't work very well!

Yet, you can try this sequence:

All NOR driver and QSPI should be put in RAM.

1- Disable Interrupts 

2- Stop scheduler (suspend)

3- Do erase/write (You should use QSPI in polling)

4- Activate MMM

5- Enable Interrupts

6- Resume Scheduler

It worked very well but wasn't stable! Sometime I get hard faults. My solution was to use an SDRAM. 

 

 

JonConesaAuthor
Associate III
April 27, 2026
Thank you for the reply.
I’ll review the options and decide which approach is best. In my case, using the MCU’s internal flash seems like the safer choice.

 

 

ST Technical Moderator
April 24, 2026

Hello @JonConesa 

Yes, this is the correct approach: temporarily exit memory-mapped mode, perform erase/program in indirect mode, then re-enable memory-mapped mode.

With ThreadX, you should serialize all external flash access using a mutex and ensure no other thread reads the mapped region while a write is in progress.

Please refer to the example below:

STM32CubeH7/Projects/STM32H745I-DISCO/Examples/QSPI/QSPI_MemoryMappedDual at master · STMicroelectronics/STM32CubeH7

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om