External flash loader for STM32H735AGIx using OCTOSPI1 on MX25LM51245g partly working
- 3 replies
- 393 views
Hello everyone,
I'm currently working on a custom board with an STM32H735AGI6, and I'm trying to create the external loader for the MX25LM51245g NOR flash on it. I use the OCTOSPI1 for the communication.
I first created a basic project using STM32CubeIDE in version 1.18.1 to validate the OCTOSPI communication and hardware of my board. And I'm able read/write the register of the external flash, as well as erasing block or full chip, and writing data into it.
Then I tried to create the external loader fallowing this tutorial : https://controllerstech.com/w25q-flash-series-part-10-qspi-ext-loader-in-h750/ adapting it to my needs.
My problem is that when I test my external loader, through the STM32CubeIDE or the STM32CubeProgrammer, by erasing the first block and writing into it, the erase goes well, but I next get the error log 'failed to download sector[0].
I debug my external loader project directly from the RAM (0x24000004) address using STM32CubeIDE, and I'm able to erase and write as well.
I attached to this post the project I use to debug the OCTOSPI com and to create the external loader.
Thanks by advance for your help !