Skip to main content
PCu1
Senior
Oct 25, 2024 6:58 PM UTC
Solved

example with analog microphone crashes on STM32F412G-Discovery

Hello, 

I'm trying to do a quick test with the STM32F412G-Discovery kit and the analogue microphone input.
I use this example https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32F412G-Discovery/Examples/BSP

with the menu #### AUDIO REC ANALOG ####.

The problem is that the firmware crashes at the line BSP_AUDIO_IN_Record(internal_buffer, AUDIO_BLOCK_SIZE);

 

void AudioRecAnalog_demo (void)
{
 AudioRec_SetHint();

 /* Initialize Audio Recorder */
 if (BSP_AUDIO_IN_InitEx(INPUT_DEVICE_ANALOG_MIC, DEFAULT_AUDIO_IN_FREQ, DEFAULT_AUDIO_IN_BIT_RESOLUTION, DEFAULT_AUDIO_IN_CHANNEL_NBR) == AUDIO_OK)
 {
 BSP_LCD_SetBackColor(LCD_COLOR_WHITE);
 BSP_LCD_SetTextColor(LCD_COLOR_GREEN);
 BSP_LCD_DisplayStringAt(0, BSP_LCD_GetYSize() - 95, (uint8_t *)" AUDIO RECORD INIT OK ", CENTER_MODE);
 }
 else
 {
 BSP_LCD_SetBackColor(LCD_COLOR_WHITE);
 BSP_LCD_SetTextColor(LCD_COLOR_RED);
 BSP_LCD_DisplayStringAt(0, BSP_LCD_GetYSize() - 95, (uint8_t *)" AUDIO RECORD INIT FAIL", CENTER_MODE);
 BSP_LCD_DisplayStringAt(0, BSP_LCD_GetYSize() - 80, (uint8_t *)" Try to reset board ", CENTER_MODE);
 }

 audio_rec_buffer_state = BUFFER_OFFSET_NONE;

 /* Display the state on the screen */
 BSP_LCD_SetBackColor(LCD_COLOR_WHITE);
 BSP_LCD_SetTextColor(LCD_COLOR_BLUE);
 BSP_LCD_DisplayStringAt(0, BSP_LCD_GetYSize() - 80, (uint8_t *)" RECORDING... ", CENTER_MODE);


 /* Start Recording */ crash here
 BSP_AUDIO_IN_Record(internal_buffer, AUDIO_BLOCK_SIZE);

 /* Wait end of one block recording */
 while((audio_rec_buffer_state & BUFFER_OFFSET_FULL) != BUFFER_OFFSET_FULL);

 /* Stop recorder */
 BSP_AUDIO_IN_Stop();

 

Does anyone have an idea?

 

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 24, 2026 1:18 PM UTC

Hello,

An update from the internal team saying that the issue is in BSP_AUDIO_IN_InitEx(uint32_t InputDevice, uint32_t AudioFreq, uint32_t BitRes, uint32_t ChnlNbr) which doesn't properly stop the DMA channel after configuring the audio codec and setting the parameters of the I2S3 peripheral. Since the DMA isn't properly disabled, it doesn't properly store the recorded data later in the buffer, and that's why the transfer isn't accomplished, and the example crushes at this stage.

This will be fixed in the coming revision of the Cube.

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

3 replies

mƎALLEm
ST Technical Moderator
Nov 5, 2024 1:20 PM UTC

Hello,

Internal ticket 195718 for follow up and confirmation of the issue / fix if there is one ..

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Nov 18, 2024 2:04 PM UTC

FYI,

Behavior reproduced internally. Analysis is ongoing.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 24, 2026 1:18 PM UTC

Hello,

An update from the internal team saying that the issue is in BSP_AUDIO_IN_InitEx(uint32_t InputDevice, uint32_t AudioFreq, uint32_t BitRes, uint32_t ChnlNbr) which doesn't properly stop the DMA channel after configuring the audio codec and setting the parameters of the I2S3 peripheral. Since the DMA isn't properly disabled, it doesn't properly store the recorded data later in the buffer, and that's why the transfer isn't accomplished, and the example crushes at this stage.

This will be fixed in the coming revision of the Cube.

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.