Skip to main content
Ss.61
Associate III
Oct 9, 2021 5:56 AM UTC
Question

Example for Usb Host Msc

Hello,

  • I am having stm32f072RB discovery board,
  • I create & save some event log in micro controller ,
  • Here i want to download the log to usb stick (Flash Drive) through usb bus feature,
  • The log format is (.txt) (saved data from NOR flash ic)
  • Micro controller act as a Host for Mass storage class

i need your help where to start the project,

if i will get example for these type of application will also help me to start this,

Thanks

regards

< siva >

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
Oct 9, 2021 6:12 AM UTC

Does the F0 even have a USB Host Controller?

​

Y​ou could look in the CubeF0 board example trees for examples. MSC devices for sure.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Ss.61
Ss.61Author
Associate III
Oct 9, 2021 9:21 AM UTC

yes,It has find the attachment,

I dont find any examples in  CubeF0 board example tree,

After check all resources i cant find any sample programs / relevant example kindly help me to find some useful resources.

Tesla DeLorean
Guru
Oct 9, 2021 9:19 PM UTC

HOST != DEVICE

For a DEVICE

STM32Cube_FW_F0_V1.10.1\Projects\STM32072B_EVAL\Applications\USB_Device\MSC_Standalone

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..