Skip to main content
Aarra.1
Associate III
Jun 28, 2022 5:14 AM UTC
Question

Ethernet packets are dropped after receiving zero.

Dear all,

I have established ethernet UDP connection using the following tutorial https://controllerstech.com/stm32-ethernet-3-udp-client/

And i'm able to transmit and receive packets.

But the problem is when my receive packet contains zero all the data after the zero packet is dropped.

Eg: If my receive packet is 123045 I'm receiving only 123 (but the data length defined is 6)

How can I solve this issue?

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
Jun 28, 2022 9:55 AM UTC

> Eg: If my receive packet is 123045 I'm receiving only 123 (but the data length defined is 6)

How do you check that, exactly?

JW