Skip to main content
vadim2
Associate II
Feb 7, 2018 12:33 PM UTC
Solved

Error in STM32 LL GPIO driver

Posted on February 07, 2018 at 13:33

Greetings. I wasted a lot of time trying to figure out what is wrong with I2Ccommunication and thus found this issue. Following code works as it is expected to (it changes corresponding CNFy bits to 0x03 and MODEy bits to 0x03 too):

 /* Configure SCL Pin as : Alternate function, High Speed, Open drain, Pull up */
 LL_GPIO_SetPinMode(GPIOB, LL_GPIO_PIN_6, LL_GPIO_MODE_ALTERNATE);
 LL_GPIO_SetPinSpeed(GPIOB, LL_GPIO_PIN_6, LL_GPIO_SPEED_FREQ_HIGH);
 LL_GPIO_SetPinOutputType(GPIOB, LL_GPIO_PIN_6, LL_GPIO_OUTPUT_OPENDRAIN);
 LL_GPIO_SetPinPull(GPIOB, LL_GPIO_PIN_6, LL_GPIO_PULL_UP);
 /* Configure SDA Pin as : Alternate function, High Speed, Open drain, Pull up */
 LL_GPIO_SetPinMode(GPIOB, LL_GPIO_PIN_7, LL_GPIO_MODE_ALTERNATE);
 LL_GPIO_SetPinSpeed(GPIOB, LL_GPIO_PIN_7, LL_GPIO_SPEED_FREQ_HIGH);
 LL_GPIO_SetPinOutputType(GPIOB, LL_GPIO_PIN_7, LL_GPIO_OUTPUT_OPENDRAIN);
 LL_GPIO_SetPinPull(GPIOB, LL_GPIO_PIN_7, LL_GPIO_PULL_UP);�?�?�?�?�?�?�?�?�?�?�?

Given:

#define RF430_NRST LL_GPIO_PIN_4
#define RF430_INT LL_GPIO_PIN_5
#define RF430_I2C_SIG LL_GPIO_PIN_8
#define RF430_I2C_RD LL_GPIO_PIN_9
#define RF430_SDA LL_GPIO_PIN_7
#define RF430_SCL LL_GPIO_PIN_6
#define RF430_IO_PORT GPIOB�?�?�?�?�?�?�?�?

Next code snippet should do the same job.However for some reason it sets CNFy bits to 0x02 and MODEy bits to 0x01, which is far from what I expect to see.

 LL_GPIO_InitTypeDef pin_init;
 pin_init.Mode = LL_GPIO_MODE_ALTERNATE;
 pin_init.OutputType = LL_GPIO_OUTPUT_OPENDRAIN;
 pin_init.Speed = LL_GPIO_SPEED_FREQ_HIGH;
 pin_init.Pull = LL_GPIO_PULL_UP;
 pin_init.Pin = RF430_SCL;
 LL_GPIO_Init(RF430_IO_PORT, &pin_init);
 pin_init.Pin = RF430_SDA;
 LL_GPIO_Init(RF430_IO_PORT, &pin_init);�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

GPIO LL driver code looks like totally unreadable mess, so I can't figure outwhetherit is my bad or issue in code. However some workaround and clarification required, I think.

#gpio #ll-gpio #ll-drivers #ll #i2c
This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Mar 22, 2018 9:00 AM UTC
Posted on March 22, 2018 at 10:00

Hello,

We would inform you that 

GPIO LL driver issue is fixed with 

the new patch of STM32CubeF1 Firmware package V1.6.1.

Kind Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

7 replies

Tilen MAJERLE
ST Employee
Feb 7, 2018 2:16 PM UTC
Posted on February 07, 2018 at 15:16

Hello

Mischuk.Vadim

‌,

can you please share which STM32 family you use and STM32Cubexx version you have?

Best regards,

Tilen

vadim2
vadim2Author
Associate II
Feb 8, 2018 10:29 AM UTC
Posted on February 08, 2018 at 10:29

 * @file stm32f1xx_ll_gpio.c
 * @author MCD Application Team
 * @version V1.1.1
 * @date 12-May-2017
 * @brief GPIO LL module driver.�?�?�?�?�?

STM32F1 cube 1.6.0. I use STM32F103RET6 MCU.

emil
Associate II
Feb 8, 2018 1:11 AM UTC
Posted on February 08, 2018 at 02:11

I can confirm that LL_GPIO_Init is broken in the latest STM32CubeMX version 4.24.0 at least for STM32F1 v1.6.0 (maybe others).

Whenever pins >= pin8 are configured the corresponding pin-8 is configured instead.

This is a very important bug because it may destroy your hardware by programming the wrong pins and connecting outputs to outputs.

Example:

  GPIO_InitStruct.Pin = LL_GPIO_PIN_13|LL_GPIO_PIN_15;

inside the function you have

  pinpos = POSITION_VAL(GPIO_InitStruct->Pin);

which uses the rbit and clz asm instructions for the 0x04a000a0 value so it returns pinpos = 5

So in the end pin 5 and 7 will be programmed instead of pins 13 and 15.

ST Technical Moderator
Feb 8, 2018 1:24 PM UTC
Posted on February 08, 2018 at 14:24

Hello,

We raisedthis issueinternally for fix.

Please refer to this discussion with same issue

https://community.st.com/0D50X00009XkhPcSAJ

Sorry for the inconvenience it may bring.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Feb 19, 2018 11:07 AM UTC
Posted on February 19, 2018 at 12:07

Hello

,

,

This issue is confirmed for LL Gpio pins and this will be fixed in the next release.

We propose thisfix with LL_GPIO_Init function for ll_gpio driver :

ErrorStatus LL_GPIO_Init(GPIO_TypeDef *GPIOx, LL_GPIO_InitTypeDef *GPIO_InitStruct){ uint32_t pinmask = 0x00000000U; uint32_t pinpos = 0x00000000U; uint32_t currentpin = 0x00000000U; /* Check the parameters */ assert_param(IS_GPIO_ALL_INSTANCE(GPIOx)); assert_param(IS_LL_GPIO_PIN(GPIO_InitStruct->Pin)); assert_param(IS_LL_GPIO_MODE(GPIO_InitStruct->Mode)); assert_param(IS_LL_GPIO_PULL(GPIO_InitStruct->Pull)); /* ------------------------- Configure the port pins ---------------- */ /* Initialize pinpos on first pin set */ pinmask = (GPIO_InitStruct->Pin & 0x00FFFF00U) >> 8 ; pinpos = POSITION_VAL(pinmask);/* Configure the port pins */ while ((pinmask >> pinpos) != 0U) { /* skip if bit is not set */ if ((pinmask & (1U << pinpos)) == 0U) { pinpos++; }/* Get current io position */ if(pinpos <8 ) { currentpin = (0x00000101U << pinpos); } else { currentpin = ((0x00010001U << (pinpos-8)) | 0x04000000U); } if (currentpin) { /* Pin Mode configuration */ LL_GPIO_SetPinMode(GPIOx, currentpin, GPIO_InitStruct->Mode); /* Pull-up Pull down resistor configuration*/ LL_GPIO_SetPinPull(GPIOx, currentpin, GPIO_InitStruct->Pull); if ((GPIO_InitStruct->Mode == LL_GPIO_MODE_OUTPUT) || (GPIO_InitStruct->Mode == LL_GPIO_MODE_ALTERNATE)) { /* Check Output mode parameters */ assert_param(IS_LL_GPIO_OUTPUT_TYPE(GPIO_InitStruct->OutputType));/* Output mode configuration*/ LL_GPIO_SetPinOutputType(GPIOx, currentpin, GPIO_InitStruct->OutputType);/* Speed mode configuration */ LL_GPIO_SetPinSpeed(GPIOx, currentpin, GPIO_InitStruct->Speed); }} pinpos++; } return (SUCCESS);}

Hope this is helpful for you.

Best Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Pavel A.
Feb 20, 2018 2:54 AM UTC
Posted on February 20, 2018 at 03:54

@Vadim If you set

LL_GPIO_InitTypeDef.Mode = LL_GPIO_MODE_ALTERNATE, you also must specify theLL_GPIO_InitTypeDef.Alternate field?

This is missing in your snippet.

-- pa

Imen.DBest answer
ST Technical Moderator
Mar 22, 2018 9:00 AM UTC
Posted on March 22, 2018 at 10:00

Hello,

We would inform you that 

GPIO LL driver issue is fixed with 

the new patch of STM32CubeF1 Firmware package V1.6.1.

Kind Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks