Skip to main content
Associate III
Jun 17, 2024 11:59 AM UTC
Solved

Error in PSSI HAL code for HAL_PSSI_Abort_DMA

I am working with an STM32U575, HAL version 1.5 and found the issue described below

(Have checked the HAL code for the H5 and H7 and these contain the same issue)

See picture below, when aborting an PSSI transfer, before checking the state on lines 1258 and 1277, the state of the PSSI is already set to HAL_PSSI_STATE_ABORT. As a result the DMA transfer is not correctly aborted since none of the two conditional paths are taken.

LVan31_0-1718625311115.png

 

Imen.DBest answer
ST Technical Moderator
Jun 21, 2024 9:36 AM UTC

Hello @LVan .31 

Thank you for having reported this issue.

I escalated your request internally for analyzing via internal ticket number: 184720.

(PS: ticket number 184720 is an internal tracking number and is not accessible or usable outside of ST)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

Imen.DBest answer
ST Technical Moderator
Jun 21, 2024 9:36 AM UTC

Hello @LVan .31 

Thank you for having reported this issue.

I escalated your request internally for analyzing via internal ticket number: 184720.

(PS: ticket number 184720 is an internal tracking number and is not accessible or usable outside of ST)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
David George
Associate III
Dec 1, 2025 2:44 PM UTC

Hello @Imen.D 

Any update on when this issue will be fixed in the HAL library?

Thank you

David

ST Technical Moderator
Dec 1, 2025 7:24 PM UTC

Hi @David George 

I will check internally the status and push to fix it in the coming release.

Sorry, for the inconvenience it may cause.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks