Skip to main content
Associate
Nov 15, 2024 2:08 PM UTC
Question

Ensure that Frequency clock is in the range [3 * baudrate, 4096 * baudrate]

Dear MCD Application Team,

in Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal_uart.c you can find this check:

/* Ensure that Frequency clock is in the range [3 * baudrate, 4096 * baudrate] */
if ((lpuart_ker_ck_pres < (3U * huart->Init.BaudRate)) ||
(lpuart_ker_ck_pres > (4096U * huart->Init.BaudRate)))
{
ret = HAL_ERROR;
}

assume huart->Init.BaudRate is 28333333 and lpuart_ker_ck_pres=170000000 the result is larger than uint32_t and results in a  HAL_ERROR

You can check this with this small test application. Maybe you can fix this in the next release.

#include <stdio.h>
#include <stdint.h>
int main() {
 uint32_t BaudRate = 28333334;
 uint32_t lpuart_ker_ck_pres = 170000000;

 printf("Start;\n");
 if (lpuart_ker_ck_pres < (3U * BaudRate))
 {
 printf("Error(1);\n");
 }
 if (lpuart_ker_ck_pres > (4096U * BaudRate))
 {
 printf("Error(2);\n");
 }
 printf("End;\n");
}

 

This topic has been closed for replies.

7 replies

Uwe Bonnes
Chief
Nov 15, 2024 2:19 PM UTC

Keep in mind the Cube is only meant as a start and will not cover  all cases.

Uwe Bonnes
Chief
Nov 15, 2024 2:22 PM UTC

However instead of

lpuart_ker_ck_pres > (4096U * huart->Init.BaudRate

( lpuart_ker_ck_pres / 4096) > huart->Init.Baudrate
 should avoid the overflow

Associate
Nov 15, 2024 3:47 PM UTC

this is my preferred solution. Maybe this find a way into the next release 

if (lpuart_ker_ck_pres > (4096U * (uint64_t)BaudRate))