Skip to main content
Associate
Aug 15, 2024 1:14 AM UTC
Question

Enable ARP Offload on STM32H745

Hi,

I try to enable the hardware ARP Offload in a STM32H745. The problem is, that it doesn't take the given IP adresse in die MACARPAR register regardless what the sequence of code is. I tryed it before and after enabling the ARPEN bit and before and after start the ETH. The adresse where the MACARAR register is, is staying at zero. Does anybody know, how to enable the ARP offload?

Here is my code and debug phenomenon:

 // Enable ARP offload
 MODIFY_REG(heth.Instance->MACCR, ETH_MACCR_ARP, 1U << ETH_MACCR_ARP_Pos);

 // Set ARP protocol address
 MODIFY_REG(heth.Instance->MACARPAR, ETH_MACARPAR_ARPPA, htonl(0xC0A8000DUL));

Jiahong_0-1723684351339.png

Best regards,

JIahong

This topic has been closed for replies.

3 replies

ST Employee
Aug 19, 2024 2:32 PM UTC

Hello @Jiahong ,

Can you share with us some details about the software and hardware configuration used for this context.

are you using a nucleo or disco or custom board?

are you using LWIP FreeRtos or you are working without networking stack and Rtos ?
if you are using Lwip the Feature of ARP offload is already implemented and you can see a working example in this link (see sections with #if LWIP_ARP in ethernetif.c)  
Regards

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JiahongAuthor
Associate
Aug 19, 2024 4:21 PM UTC

Hi @STea ,

Thanks for your reply. I use custom board and the hal driver version is v1.10.0. And I am implementing the udp protocol without the rtos and the lwip.

I call the HAL_ETH_ReadData() directly to get the ethernet frame and parse the udp payload by myself, and sending is similar. 

Here is my Init function:

void MX_ETH_Init()
{
 static uint8_t MACAddr[6];

 heth.Instance = ETH;
 MACAddr[0] = 0x00;
 MACAddr[1] = 0x80;
 MACAddr[2] = 0xE1;
 MACAddr[3] = 0x00;
 MACAddr[4] = 0x00;
 MACAddr[5] = 0x00 + read_address();
 heth.Init.MACAddr = &MACAddr[0];
 heth.Init.MediaInterface = HAL_ETH_MII_MODE;
 heth.Init.TxDesc = DMATxDscrTab;
 heth.Init.RxDesc = DMARxDscrTab;
 heth.Init.RxBuffLen = ETH_RX_BUFFER_SIZE;

 // Init PHY 
 HAL_GPIO_WritePin(ENETRST_N_Port, ENETRST_N_Pin, GPIO_PIN_SET); 

 if (HAL_ETH_Init(&heth) != HAL_OK)
 {
 Error_Handler();
 }

 memset(&TxConfig, 0 , sizeof(ETH_TxPacketConfig));
 TxConfig.Attributes = ETH_TX_PACKETS_FEATURES_CSUM;
 TxConfig.ChecksumCtrl = ETH_CHECKSUM_IPHDR_PAYLOAD_INSERT_PHDR_CALC;
 TxConfig.CRCPadCtrl = ETH_CRC_INSERT;

 // Get MAC Config MAC
 ETH_MACConfigTypeDef MACConf = {0};
 HAL_ETH_GetMACConfig(&heth, &MACConf);
 MACConf.DuplexMode = ETH_FULLDUPLEX_MODE;
 MACConf.Speed = ETH_SPEED_100M;
 HAL_ETH_SetMACConfig(&heth, &MACConf);

 // Set the MAC filter to reject sendor MAC adderss: 00-08-e1-xx-xx-xx
 HAL_ETH_GetMACFilterConfig(&heth, &MacFilterConfig);
 MacFilterConfig.SrcAddrFiltering = ENABLE;
 MacFilterConfig.SrcAddrInverseFiltering = ENABLE;
 HAL_ETH_SetMACFilterConfig(&heth, &MacFilterConfig);

 // Config the ETH_MAC_ADDRESS1 register
 // Enable source filter
 MODIFY_REG(heth.Instance->MACA1HR, ETH_MACA1HR_AE, 1U << ETH_MACA1HR_AE_Pos);
 MODIFY_REG(heth.Instance->MACA1HR, ETH_MACA1HR_SA, 1U << ETH_MACA1HR_SA_Pos);
 // Config mac address
 MODIFY_REG(heth.Instance->MACA1HR, ETH_MACA1HR_ADDRHI, MACAddr[5] << 8U | MACAddr[4]);
 MODIFY_REG(heth.Instance->MACA1LR, ETH_MACA1LR_ADDRLO, *((uint32_t*)(MACAddr)));
 // Config mask to check the 3 MSB
 MODIFY_REG(heth.Instance->MACA1HR, ETH_MACA1HR_MBC, 7U << (ETH_MACA1HR_MBC_Pos + 3U));

 MODIFY_REG(heth.Instance->MACHWF0R, ETH_MACHWF0R_ARPOFFSEL, ETH_MACHWF0R_ARPOFFSEL);
 MODIFY_REG(heth.Instance->MACCR, ETH_MACCR_ARP, 1U << ETH_MACCR_ARP_Pos);
 MODIFY_REG(heth.Instance->MACARPAR, ETH_MACARPAR_ARPPA, htonl(0xC0A8000DUL));

 HAL_ETH_Start_IT(&heth);
}

 

 

ST Employee
Sep 26, 2024 10:31 AM UTC

Hello @Jiahong ,

did you manage to solve this issue.

my recommendation is to have incremental changes out of the MX_eth_init function 
this sequence is not described in RM so it could be the one causing

 HAL_ETH_GetMACFilterConfig(&heth, &MacFilterConfig);
 MacFilterConfig.SrcAddrFiltering = ENABLE;
 MacFilterConfig.SrcAddrInverseFiltering = ENABLE;
 HAL_ETH_SetMACFilterConfig(&heth, &MacFilterConfig);

 // Config the ETH_MAC_ADDRESS1 register
 // Enable source filter
 MODIFY_REG(heth.Instance->MACA1HR, ETH_MACA1HR_AE, 1U << ETH_MACA1HR_AE_Pos);
 MODIFY_REG(heth.Instance->MACA1HR, ETH_MACA1HR_SA, 1U << ETH_MACA1HR_SA_Pos);
 // Config mac address
 MODIFY_REG(heth.Instance->MACA1HR, ETH_MACA1HR_ADDRHI, MACAddr[5] << 8U | MACAddr[4]);
 MODIFY_REG(heth.Instance->MACA1LR, ETH_MACA1LR_ADDRLO, *((uint32_t*)(MACAddr)));
 // Config mask to check the 3 MSB
 MODIFY_REG(heth.Instance->MACA1HR, ETH_MACA1HR_MBC, 7U << (ETH_MACA1HR_MBC_Pos + 3U));

 MODIFY_REG(heth.Instance->MACHWF0R, ETH_MACHWF0R_ARPOFFSEL, ETH_MACHWF0R_ARPOFFSEL);
 MODIFY_REG(heth.Instance->MACCR, ETH_MACCR_ARP, 1U << ETH_MACCR_ARP_Pos);
 MODIFY_REG(heth.Instance->MACARPAR, ETH_MACARPAR_ARPPA, htonl(0xC0A8000DUL));

Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.