Skip to main content
mete
Senior
Sep 11, 2023 6:56 PM UTC
Solved

eh_frame, init and fini in a C build

I see these in the linker scripts, but I do not see them in the output for a C application.

I know eh_frame is for C++ exceptions, and it is not strange it is not in the output of the C application. I also read it is used for some C functionality as well. Can these functionality be used in embedded platforms (without an OS) ? Can I ever see eh_frame in a C build output ?

I thought init and fini is only for processes and shared objects. Neither is in a C project, are these used for anything else ? 

This topic has been closed for replies.
Issamos
IssamosBest answer
Super User
Sep 11, 2023 7:18 PM UTC

Hello @mete 

you might still encounter eh_frame sections if certain C features that require stack unwinding support bit. But, this is going to be rare.

For init and fini, I don't think they have uses other than what you said.

Best regards.

II

4 replies

Issamos
IssamosBest answer
Super User
Sep 11, 2023 7:18 PM UTC

Hello @mete 

you might still encounter eh_frame sections if certain C features that require stack unwinding support bit. But, this is going to be rare.

For init and fini, I don't think they have uses other than what you said.

Best regards.

II

mete
meteAuthor
Senior
Sep 11, 2023 7:41 PM UTC

Thanks @Issamos , is there a documentation about when eh_frame is used in C ? or does C standard or GNU toolchain mandate the support/inclusion of eh_frame ? 

Issamos
Super User
Sep 11, 2023 7:54 PM UTC

I suggest you to take a look at this post.

Best regards.

II