Skip to main content
Associate II
Nov 5, 2023 2:44 PM UTC
Solved

EEPROM emulation problem on STM32H563

Hi,

I'm facing problem in reading data from EEPROM, which was written before power cycle.
EE_Init() always causes formatting of EEPROM irrespective of EE_CONDITIONAL_ERASE or EE_FORCED_ERASE parameter passed, resulting in erasing the previous data
Configuration: "STM32H5 series using high-cycle data area" with EDATA_ENABLED & START_PAGE_ADDRESS 0x0900C000U

I'm using the latest version of EEPROM emulation driver "X-CUBE-EEPROM version-6.0.0" on dev kit "NUCLEO-H563ZI"

The example code works fine, it is able to write and read the data from the flash every time on power up by formatting the page, but when I wanted to read the data which was written in previous cycle, It always reads data zero.

The reason I found was, it always give current page status as "ERASING".

I made the following change in function FindPage(), having a switch case operation for "FIND_READ_PAGE" by adding a check currentpagestatus == STATE_PAGE_VALID as shown below.

I added STATE_PAGE_VALID check instead of STATE_PAGE_ERASING, because, the debugger shows the current page status as valid in function FindPage()

case FIND_READ_PAGE: /* ---- Read operation ---- /
if (currentpagestatus == STATE_PAGE_ACTIVE || currentpagestatus == STATE_PAGE_VALID)
{
     return currentpage;
}
else
{
    if (currentpagestatus == STATE_PAGE_RECEIVE)
    {
         return previouspage;
    }
    else
    {
         return EE_NO_PAGE_FOUND; / No active Page */
    }
}

In main.c I added the following code just before initializing the EE_Init
ConfigureCrc();
for (Index = 1; Index < NB_OF_VARIABLES+1; Index++)
{
    EE_ReadVariable32bits(Index, &a_VarDataTab[Index-1]);
}
with the above change I'm now able to read data which was written in previously.

Am I missing some settings? please help!

This topic has been closed for replies.
Florian LR
Florian LRBest answer
ST Employee
Nov 6, 2023 9:43 AM UTC

Hi @Bhuvi-Naveen, and welcome to the STCommunity !

Thank you for reporting us the issue, we already identified it on our side, and the patched version of the firmware will be released in the next days.

This is happening because NMIs are triggered during the step 1 of EE_Init().

You can already patch it on your side, before the firmware update.

In the file stm32h5xx_it.c in function NMI_Handler, add the following lines after
 if (__HAL_FLASH_GET_FLAG(FLASH_FLAG_ECCD)) { : 

 

#ifdef EDATA_ENABLED
 if (READ_REG(FLASH->ECCDR) == 0xFFFF)
 {
 __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_ECCD);
 return;
 }
#endif

 


If you have any issue, please don't hesitate to come back. 
Best Regards,

Florian LR

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

Florian LR
Florian LRBest answer
ST Employee
Nov 6, 2023 9:43 AM UTC

Hi @Bhuvi-Naveen, and welcome to the STCommunity !

Thank you for reporting us the issue, we already identified it on our side, and the patched version of the firmware will be released in the next days.

This is happening because NMIs are triggered during the step 1 of EE_Init().

You can already patch it on your side, before the firmware update.

In the file stm32h5xx_it.c in function NMI_Handler, add the following lines after
 if (__HAL_FLASH_GET_FLAG(FLASH_FLAG_ECCD)) { : 

 

#ifdef EDATA_ENABLED
 if (READ_REG(FLASH->ECCDR) == 0xFFFF)
 {
 __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_ECCD);
 return;
 }
#endif

 


If you have any issue, please don't hesitate to come back. 
Best Regards,

Florian LR

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Associate II
Nov 6, 2023 5:20 PM UTC

Hello Florian,

Thank you for your quick response!

It is working fine after adding the above patch.

Regards,

Bhuvi-Naveen

Explorer
Dec 5, 2023 8:50 AM UTC

Thank you for explanation.

 

BR,

Maxi

Senior
Mar 26, 2024 6:29 AM UTC

Just  install my pack and enjoy.

https://github.com/nimaltd/ee