Skip to main content
Visitor II
Jul 23, 2025 9:20 AM UTC
Question

Dual Core Debug on STM32H755

I'm developing a project with the dual-core STM32h755zi-q, but when I run the m4 core while debugging, I encounter the error, "Break at address "0xa05f0000" with no debug information available, or outside of program code." I've configured the debugging settings according to the documentation and video shared by ST. I'm currently working on the m4 core, and I'll switch to the m7 core later, but I'm not making any progress due to the error I mentioned above.I would like to express my gratitude to everyone who helped.

Screenshot 2025-07-23 at 12.16.20.png

This topic has been closed for replies.

2 replies

CTapp.1
Senior III
Jul 23, 2025 2:41 PM UTC

I'm seeing the same with an H757 device and IDE V 1.19.1.

The debugger loads the code and stops at main(), as expected. I can single step from there, but I get the message you reported if I run to a breakpoint.

The stack window shows:

[core: 3]( Suspended : Signal : SIGTRAP:Trace/breakpoint trap)

I get the same if I just hit run after loading with no breakpoints set. 

All posts are made in a personal capacity. MISRA C++ Chair, MISRA C WG Member, Director The MISRA Consortium Limited (TMCL)
ST Technical Moderator
Jul 28, 2025 10:02 AM UTC

Hello @oppressive08 

Please refer to the application note below to configure the STM32CubeIDE for dual core debug:

Getting started with projects based on dual-core STM32H7 microcontrollers in STM32CubeIDE - Application note

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om