Skip to main content
Associate II
May 16, 2025 12:04 PM UTC
Question

Dual Bootloader with FDCAN Firmware Update and CRC Validation on STM32G0B1CCT6

I am working on a custom dual-boot bootloader for the STM32G0B1CCT6 with the following features:

  • Bootloader located at 0x08000000 (about 20 KB flash).

  • Two application firmware slots:

    • App1 at 0x08005000 (22 KB)

    • App2 at 0x0800A800 (22 KB)

  • On reset, the bootloader checks the CRC of App1 and App2 firmware:

    • If App1 is valid, it jumps to App1.

    • Else if App2 is valid, it jumps to App2.

    • Else it stays in bootloader mode.

  • Firmware updates are sent via FDCAN as .bin files (no special commands, just the binary data).

  • The bootloader receives the firmware, writes it to the free app slot, verifies CRC:

    • If CRC passes, it overwrites the old firmware and jumps to the new app.

    • If CRC fails, it keeps the old firmware and stays in bootloader mode.

  • I want to support multiple firmware updates this way reliably.

I have basic HAL code generated from CubeMX for FDCAN and CRC peripherals.

My questions:

  1. Is my memory layout and CRC validation approach suitable for STM32G0B1CCT6 with 64KB flash?

  2. How can I best implement the FDCAN reception to reliably receive large .bin files chunked over CAN FD?

  3. Are there any reference projects or examples from ST that implement similar dual-bootloader with CRC check and FDCAN update?

  4. Any tips on safely erasing and writing flash while receiving firmware over FDCAN?

  5. How do I store and update CRC metadata securely in flash?

  6. How to properly jump from bootloader to application and manage vector tables?

This topic has been closed for replies.

10 replies

Associate II
May 16, 2025 10:43 AM UTC

Problem Statement:

I am developing a custom bootloader for the STM32G0B1CCT6 microcontroller that supports the following functionality:

  1. Dual Boot Mode:

    • The bootloader is programmed via ST-LINK V2.

    • The application firmware is uploaded later via FDCAN in .bin format.

  2. CRC Validation:

    • On every power-up or reset, the bootloader checks the CRC of the existing application firmware.

    • If the firmware is valid (CRC matches), the bootloader jumps to the application.

    • If the firmware is invalid (CRC mismatch or corrupted), the bootloader remains active and does not jump.

  3. Firmware Update via FDCAN:

    • The bootloader receives the new .bin file via FDCAN (without waiting for any specific command/message).

    • After receiving the complete firmware, it calculates the CRC and verifies it.

    • If the new firmware is valid, the bootloader erases the previous one and flashes the new firmware.

    • If the new firmware is invalid, the old firmware remains untouched and continues to run.

  4. Repeatable Process:

    • I should be able to update the firmware multiple times via FDCAN.

    • Each time, CRC is verified before replacing the existing firmware.

Goal:
To ensure reliable firmware updates via FDCAN, with automatic CRC verification and fallback to the previous valid firmware if the update fails or is corrupted.

ST Technical Moderator
May 16, 2025 12:43 PM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
AKG123Author
Associate II
May 17, 2025 4:05 AM UTC

Thank you for the reference.

I did check the example at:
STM32CubeG4/Projects/NUCLEO-G491RE/Applications/OpenBootloader,
but I was not able to fully understand it.

If there is any specific example for FDCAN or CAN-based bootloader (especially for STM32G0 series) available on GitHub or any official ST repo, could you please share the link? That would be very helpful.

ST Technical Moderator
May 19, 2025 8:07 AM UTC

Hello @AKG123 

There is a CAN bootloader driver, it can be useful for your application.

stm32-mw-openbl/Modules/CAN/openbl_can_cmd.c at main · STMicroelectronics/stm32-mw-openbl · GitHub

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om