Skip to main content
TLeut
Visitor II
April 23, 2019
Question

Dual Boot into ITCM-flash

  • April 23, 2019
  • 0 replies
  • 449 views

Hello,

dual boot into ITCM-flash doesn't work like I do it.

Dual Boot into AXIM-flash works.

With OpenOCD I do the following for boot from AXIM-flash:

Boot adddress is 0x8010000 (boot_addr = 0x2004)

> stm32f2x options_write 0 0xCFC 0x2004 0x2004
 
> stm32f2x options_read 0
stm32f2x user_options 0xCFC, boot_add0 0x2004, boot_add1 0x2004

Content of relevant boot addresses (SP and reset handler):

> mdw 0x08010000 2
0x08010000: 20020000 08010239

Breakpoint at reset handler and check if breakpoint is reached:

> bp 0x08010239 2 hw
breakpoint set at 0x08010239
> reset
adapter speed: 2000 kHz
target halted due to breakpoint, current mode: Thread
xPSR: 0x21000000 pc: 0x08010238 msp: 0x20020000

Same for ITCM-flash

Boot adddress is 0x210000 (boot_addr = 0x84)

> stm32f2x options_write 0 0xCFC 0x84 0x84
 
> stm32f2x options_read 0
device id = 0x10006451
flash size = 2048kbytes
Dual Bank 2048 kiB STM32F76x/77x found
stm32f2x user_options 0xCFC, boot_add0 0x0084, boot_add1 0x0084

Content of relevant boot addresses (SP and reset handler):

> mdw 0x08010000 2
0x08010000: 20020000 00210239

Breakpoint at reset handler and check if breakpoint is reached:

> bp 0x00210239 2 hw
breakpoint set at 0x00210239
> reset
adapter speed: 2000 kHz

No stop at breakpoint as bootloader is started.

Value at OPTCR and OPTCR1 register:

> mdw 0x40023C14 2
0x40023c14: cfffaafd 20042004

What do I wrong?

Regards

Tobias

This topic has been closed for replies.