Skip to main content
RLeva.1
Visitor II
Nov 26, 2021 3:51 PM UTC
Question

Dual Bank Live Firmware Update and EEPROM emulation

Hi Forum,

Is there any example using stm32 ARM MCUS that implements the "Dual Bank " on the fly firmware update and EEPROM emulation in the SAME application?

See :

https://www.st.com/resource/en/application_note/dm00230416-onthefly-firmware-update-for-dual-bank-stm32-microcontrollers-stmicroelectronics.pdf

to understand Dual bank Firmware Update On the Fly

Thank you

This topic has been closed for replies.

1 reply

Bubbles
ST Employee
Dec 7, 2021 2:33 PM UTC

Hi @RLeva.1​ ,

no there is not. Most examples try to focus on single topic and it would make it more difficult to comprehend if there were these two combined.

But there is no obvious obstacle preventing use of these two combined. Unlike for example trying to combine SBSFU and OTFU would be impossible.

If you have any specific problem with combination of EEPROM emulation and OTF update let me know. But it should be easy.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.