Skip to main content
SWood.8
Associate II
January 24, 2019
Question

Download of latest STM32Cube MCU Package examples for STM32H7 (en.stm32cubeh7_v_1-3-1.zip) is empty / corrupted / only 5Kb

  • January 24, 2019
  • 6 replies
  • 1665 views

Whereas selecting v1.3.0 downloads the full ~400Mb file. Anyone else having this problem ?

This topic has been closed for replies.

6 replies

ST Technical Moderator
January 24, 2019

Hello,

Thanks for highlighting this issue. We are working to resolve this.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
January 25, 2019

Hello @SWood.8​ ,

This issue is fixed now and you can download the patch release v1.3.1.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
SWood.8
SWood.8Author
Associate II
January 25, 2019

Great : ) will do

After Forever
Senior III
January 25, 2019

It still doesn't show up in STM32CubeMX's "Check for Updates" list for me. Or maybe minor updates are not being listed there?

redmig
Associate III
February 12, 2019

This is the situation today:

en.stm32cubeh7.zip --> v1.3.0 --> OK (394 MB)

en.stm32cubeh7_v_1-3-1 --> v1.3.1 --> CORRUPTED FILE - NOT OK! (4.93KB)

en.patch_cubeh7.zip --> v1.3.2 --> OK (1.14MB)

Question is: can we skip v1.3.1 and use directly 1.3.2?

Thanks

ST Technical Moderator
February 12, 2019

Hello,

You should use the new patch of STM32CubeH7 V1.3.2, which englobe new fix of UID_BASE definition to the CMSIS STM32H7xx include files and also the fix of LwIP and mbedTLS applications (added in the v1.3.1 patch) 

The patch v1.3.1 will be removed from the ST web site.

Kind Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks