Skip to main content
FPicc
Visitor II
May 11, 2019
Question

Does the STM32F303 USB require an external termination series resistor?

  • May 11, 2019
  • 0 replies
  • 613 views

In the STM32F303 datasheet is written that "no external termination series resistor are required on USB_D+ and USB_D-, the matching impedance is already included in the embedded driver." However, if I look at the STM32F3DISCOVERY board I see 22 Ohm termination series resistors before the CN2 (USB-USER connector).Do I need them in my design or not? Is it necessary also to design the signal traces in the PCB in order to show a particular characteristic impedance?

This topic has been closed for replies.