Skip to main content
NM.1
Associate II
Jul 14, 2022 1:11 PM UTC
Solved

Does STM32U585 supports USB RNDIS ?

Hi All,

I am starting work on USB RNDIS support for STM32U5, and completely new to this.

I am looking for example/documentation on USB RNIDS support on STM32U5.

Can anyone please help here ?

This topic has been closed for replies.
KHors.1
KHors.1Best answer
Associate
Jul 19, 2022 8:27 AM UTC

The RNDIS class is provided with STM32Cube.

You can find it under ...\STM32Cube\Repository\<Your library and version>\Middlewares\ST\STM32_USB_Device_Library\Class\CDC_RNDIS.

A good starting point would be a CDC virtual serial port project, then modify it to the RNDIS structures und modules. The basic structure and calls are pretty similar.

Documentation for the RNDIS class (and all others) is here wiki.st.com/stm32mcu/wiki/Introduction_to_USB_with_STM32#CDC_Remote_Network_Driver_Interface_Specification_-28RNDIS-29_Sublass.

If the class is not provided for STM32U5 MCUs you can "steal" it from another models, like L4 or F4. Just install the Cube support for one of these, parallel to the U5 library.

The effort on integrating the stuff, and making it work is however completely on your side.

3 replies

ST Technical Moderator
Jul 15, 2022 1:59 PM UTC

Hello @NM.1​ ,

There is no RNDIS example within STM32CubeU5 MCU package.

You may use examples provided on Microsoft Azure RTOS repo in order to develop your own RNDIS application.

We are currently working on adding multiple USBX classes to our packages including RNDIS.

Thank you for your understanding and your contribution.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
KHors.1
KHors.1Best answer
Associate
Jul 19, 2022 8:27 AM UTC

The RNDIS class is provided with STM32Cube.

You can find it under ...\STM32Cube\Repository\<Your library and version>\Middlewares\ST\STM32_USB_Device_Library\Class\CDC_RNDIS.

A good starting point would be a CDC virtual serial port project, then modify it to the RNDIS structures und modules. The basic structure and calls are pretty similar.

Documentation for the RNDIS class (and all others) is here wiki.st.com/stm32mcu/wiki/Introduction_to_USB_with_STM32#CDC_Remote_Network_Driver_Interface_Specification_-28RNDIS-29_Sublass.

If the class is not provided for STM32U5 MCUs you can "steal" it from another models, like L4 or F4. Just install the Cube support for one of these, parallel to the U5 library.

The effort on integrating the stuff, and making it work is however completely on your side.

NM.1
NM.1Author
Associate II
Jul 22, 2022 1:07 PM UTC

Thank you so much @Imen DAHMEN​  and @KHors.1​  for your inputs.

This will work for me.

:grinning_face: