Skip to main content
ALin.6
Associate
Nov 17, 2023 2:20 AM UTC
Question

Does stm32f107 support with en.STM32CubeExpansion_Crypto?

I'm try to develop encryption functionality. 
Two optionnal,

1. stm32  lib  "en.STM32CubeExpansion_Crypto"
2. mbedtls 
So I have to question about it. 
1.  Does stm32F107 support "en.STM32CubeExpansion_Crypto".

2.  If were you, which option do you have? 

This topic has been closed for replies.

2 replies

ALin.6
ALin.6Author
Associate
Nov 17, 2023 2:23 AM UTC

If select mbedtls seems RAM not big enough. 

ST Employee
Nov 17, 2023 9:45 AM UTC

Hello @ALin.6 ,

you can use the en.STM32CubeExpansion_Crypto it's available across all STM32 series. For the STM32F107 you can use the libSTM32Cryptographic_CM3.a available in the x-cube-cryptolib package.

You can follow the following tutorial to see how to integrate the library into your project .

BR 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.