Skip to main content
Lmatt.11
Associate III
Jan 20, 2022 7:55 AM UTC
Solved

Does somebody do the debugging and tests on these two EVM: board NUCLEO-G0B1RE + X-NUCLEO-USBPDM1?

  • Configure as a extended capacity SINK(15V/3A)
  • NUCLEO-G0B1RE + X-NUCLEO-USBPDM1
  • Could somebody can share some documents for reference?
  • or if can give some suggestions or advices , it's also graet!
This topic has been closed for replies.
Nicolas P.
Nicolas P.Best answer
ST Employee
Feb 23, 2022 7:22 AM UTC

Hello @Lmatt.1​ 

have a look at this wiki, il will show how to use the UM2552 (stack user manual). The UCPD monitor tool is very convenient to trigger some actions, and see what's going on the protocol side.

You can also have a look at this wiki to see how to do sink application step by step.

Regards,

Nicolas

9 replies

Alfredo
Associate II
Feb 18, 2022 11:14 AM UTC

Yes, I use this board for USB-PD. What is your question ?

Lmatt.11
Lmatt.11Author
Associate III
Oct 31, 2023 3:27 PM UTC

@Alfredo ,

Do you met only one orientation of USB type C can be worked when there is a battery pack in the system?

If no battery, both orientations works fine, out put 20V/5A, or other PDO?

Thanks,

Matt

Alfredo
Associate II
Nov 5, 2023 8:58 AM UTC

I would like to help you, but I do not understand your question.

Would you mind giving me more details ?

Thanks.

Nicolas P.
Nicolas P.Best answer
ST Employee
Feb 23, 2022 7:22 AM UTC

Hello @Lmatt.1​ 

have a look at this wiki, il will show how to use the UM2552 (stack user manual). The UCPD monitor tool is very convenient to trigger some actions, and see what's going on the protocol side.

You can also have a look at this wiki to see how to do sink application step by step.

Regards,

Nicolas

Lmatt.11
Lmatt.11Author
Associate III
Feb 23, 2022 7:28 AM UTC

Hello @Nicolas P,

I have already finished the debug and tests for this combination.

The function was realized.

Thanks a lot for your reply.

Regards,

Matt

Nicolas P.
ST Employee
Oct 30, 2023 11:08 AM UTC

Hello @Lmatt.11 . I saw that you opened the same topic on an another post : https://community.st.com/t5/stm32-mcus-products/when-to-enable-the-dead-battery-mode-for-ucpd-there-are-a/m-p/602597#M226007

I propose to close this one, not to duplicate answers. Do you agree ?

Nicolas

Lmatt.11
Lmatt.11Author
Associate III
Oct 30, 2023 10:55 PM UTC

@Nicolas P. 

Yes, of course. thanks!

 

Matt