Skip to main content
AlbertoGarlassi
Associate II
March 3, 2023
Question

Does HAL callbacks save r0-r3 registers? Is it needed?

  • March 3, 2023
  • 18 replies
  • 3640 views

Hello,

We have random HardFaults on an STM32H750, maybe after several hours of uptime.

It seems caused by an access to a wrong RAM location, whose address is fetched from the stack and stored in r2.

But the stack seems OK.

This happens in a function frequently interrupted by a higher priority HAL DMA callback.

Inspecting it AFAIK registers r0-r3 are not preserved by GCC optimized at -O2.

It could be that sometimes this interrupt takes place between loading of r2 and its use, overwriting it with a wrong value.

Inside my callback function there are calls to other functions. Is this OK? I read somewhere that GCC saves only the registers it uses in the main function of the ISR and doesn't take care of register's use in called function. Don't know if it makes sense.

Adding __attribute__((interrupt)) does not seem to make any difference.

For now I added push and pop of the scratch registers in the callback and it seems to work, but I'm not completely sure because a slight timing difference could be enough to mask the problem.

It is also inconvenient, because the HAL library needs to be patched.

I am not convinced of anything I wrote before because it would break most code and it would have been spotted long ago.

Any comment?

Thanks and regards.

Alberto

This topic has been closed for replies.

18 replies

KnarfB
Super User
March 3, 2023

The callback will be at 3rd or so stack nesting levels below the native interrupt handler. So it would be way to late doing any interrupt related register fixing here. Using floating point requires special attention. Some 64-bit or larger non-atomic assignments that lead to temporarily inconsistent values?

In general, no special coding rules are needed for interrupt handlers, see https://interrupt.memfault.com/blog/arm-cortex-m-exceptions-and-nvic for a nice intro.

[Edit:] gcc has some (intrusive) stack-protection features, see https://gcc.gnu.org/onlinedocs/gcc-10.4.0/gcc/Instrumentation-Options.html

Here is some simple code to pre-fill the stack area with some magic value for diy dynamic stack size analysis:

{
 extern uint32_t _estack;
 register char * stack_ptr asm("sp");
 char * heap_top = _sbrk(0);
 printf("stack: min: %p curr: %p top: %p\n\r", heap_top, stack_ptr, &_estack );
 
 for( uint8_t *p = heap_top+4; p < stack_ptr; p++ ) {
 *p = 0xa5;
 }
}

hth

KnarfB

gbm
Super User
March 3, 2023

There is some error in your code, probably resulting from using an incorrect pointer value or a conflict between declared and actual function argument type (.h file not matching .c function declaration). Check the warnings - there should be none reported by the compilers.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
waclawek.jan
Super User
March 3, 2023

> It seems caused by an access to a wrong RAM location, whose address is fetched from the stack and stored in r2.

> But the stack seems OK.

Show.

> Inside my callback function there are calls to other functions.

printf()?

JW

Tesla DeLorean
Guru
March 3, 2023

There isn't an interrupt attribute because the MCU core pushes R0 thru R3 and LR, etc as the NVIC pulls the Handler entry from the vector table.

​

I 'd say look elsewhere for stack corruption, either out-of-bound or excessive local/auto variable depth.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
S.Ma
Principal
March 4, 2023

First sanity check would be stack size.

Second would be functions using global/static variables

Third would be variables which would require volatile yet aren't.

AlbertoGarlassi
Associate II
March 4, 2023

Thanks for your attention.

Next week I will check your kind advices.

For now please have a look at these screenshots, The first is after placing a breakpoint on the one and only line that sometimes triggers the Hardfault.

The second is taken after a Hardfault. As you can see sp is the same, the stack looks OK, r2 is loaded at 0x0800ffd8 but something happens before reaching 0x800ff4.

Since r2 is, as brilliantly pointed out, automatically saved in ISRs, the only way to achieve this I can imagine is that in some way there is a jump from somewhere landing exactly there, and the ldr r2 line is never executed. Hard to believe because, apart from this hardfault, the board performs normally, and by patching with push or shuffling the code it runs forever.

Some details I omitted:

The lower priority function where the hardfault happens is an ISR too, called by a software interrupt from the higher priority ISR,.

We have a fast, high priority DMA triggered ISR that acquires a buffer filled by DMA with data from ADC. This buffer is decimated and the result is written as a single entry in another array. The ISR returns.

When, after 512 fast ISRs the output array is complete, the lower priority function is triggered to be executed by an EXTI->SWIER1 software interrupt request, at a later time.

In other word we have a long, low priority ISR interrupted several times by the fast IRQ.

Things are somewhat more complicated because the code of the hardfault comes precompiled from the CMSIS library. I grabbed the source code and used it in a C file and it didn't trigger the hardfault, but who knows.

Yes, floating point is heavily used in both ISRs.

I-Cache and D-Cache are enabled. Hopefully are correctly invalidated when needed. Don't know if it matters.

There are other ISR and DMA transfers taking place. USB CDC is used.

Thanks for now.

0693W00000aIBoHQAW.png0693W00000aIBoMQAW.png 

Piranha
Principal III
March 5, 2023

> I-Cache and D-Cache are enabled. Hopefully are correctly invalidated when needed. Don't know if it matters.

That means it almost definitely is not maintained correctly.

https://community.st.com/s/question/0D53W00001Z9K9TSAV/maintaining-cpu-data-cache-coherence-for-dma-buffers

waclawek.jan
Super User
March 4, 2023

I don't understand the second screenshot: is this something resulting from "walkback"? I don't use Eclipse. Show us content of registers, stack, disasm at the hardfault.

JW

S.Ma
Principal
March 5, 2023

Try to disable the cache(s) function for differentilal diagnostic.

AlbertoGarlassi
Associate II
March 6, 2023

I'm checking your clues, really appreciated.

The second screenshot is from Eclipse indeed. It should bring the infos you are asking for. If you need a text file format let me know. Yes, I walked back to the hard fault context by pointing its line in the stack call view, center left. The important thing anyway is that r2 changes value without apparent reasons and triggers a hard fault while executing vldr s14, [r2].

Most promising hint is about cache. I would expect a corrupted stack and this is not the case.

Another thing I'm going to try is to disable interrupts during the CMSIS fft that gives trouble.

Regards

Alberto

ST Technical Moderator
March 7, 2023

Hello @AlbertoGarlassi​ 

It is possible that this behavior occurs and triggers a Hard Fault:

R2 is initially loaded with the address of a memory location that contains the data needed for the FFT calculation. However, if an interrupt occurs at a critical time between the load of R2 and the execution of VLDR S14, [R2], the interrupt could change the value of R2 to point to an invalid or unexpected memory location.

It's important to ensure that the software interrupt and lower priority ISR are properly configured and managed to avoid issues with timing and resource conflicts.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL