Skip to main content
MNapi
Senior II
November 8, 2024
Solved

does anybody have source code for LG4571 display (480 x 800)

there is nothing on  github.

 

there is initialization by SPI before the LTDC works

is there a sequence like you initialize it first over SPI then

MX_LTDC_Init() or it does not matter

I do have the initialization code but I am missing something

void SLGDP4571_Int(void)
{

SPI_WriteComm(0x20);

SPI_WriteComm(0x3A);
SPI_WriteData(0x70);

SPI_WriteComm(0xB1);
SPI_WriteData(0x10);
SPI_WriteData(0x14);
SPI_WriteData(0x06);

SPI_WriteComm(0xB2);
SPI_WriteData(0x00);
SPI_WriteData(0xC8);

SPI_WriteComm(0xB3);
SPI_WriteData(0x11);
SPI_WriteData(0xFF);

SPI_WriteComm(0xB4);
SPI_WriteData(0x10);

SPI_WriteComm(0xB6);
SPI_WriteData(0x08);
SPI_WriteData(0x18);
SPI_WriteData(0x02);
SPI_WriteData(0x40);
SPI_WriteData(0x10);

SPI_WriteComm(0xB7);
SPI_WriteData(0x00);
SPI_WriteData(0x10);
SPI_WriteData(0x01);

SPI_WriteComm(0xC3);
SPI_WriteData(0x04);
SPI_WriteData(0x05);
SPI_WriteData(0x04);
SPI_WriteData(0x04);
SPI_WriteData(0x01);

SPI_WriteComm(0xC4);
SPI_WriteData(0x22);
SPI_WriteData(0x03);
SPI_WriteData(0x00);
SPI_WriteData(0x1A);
SPI_WriteData(0x1A);
SPI_WriteData(0x05);
SPI_WriteData(0x00);
SPI_WriteData(0x04);

SPI_WriteComm(0xC5);
SPI_WriteData(0x6C);

SPI_WriteComm(0xC6);
SPI_WriteData(0x23);
/****
SPI_WriteComm(0xC8);
SPI_WriteData(0x01);
SPI_WriteData(0x01);
SPI_WriteData(0x03);
SPI_WriteData(0xFF);
***/

SPI_WriteComm(0xD0);
SPI_WriteData(0x00);
SPI_WriteData(0x43);
SPI_WriteData(0x64);
SPI_WriteData(0x25);
SPI_WriteData(0x10);
SPI_WriteData(0x02);
SPI_WriteData(0x71);
SPI_WriteData(0x44);
SPI_WriteData(0x04);

SPI_WriteComm(0xD1);
SPI_WriteData(0x00);
SPI_WriteData(0x43);
SPI_WriteData(0x64);
SPI_WriteData(0x25);
SPI_WriteData(0x10);
SPI_WriteData(0x02);
SPI_WriteData(0x71);
SPI_WriteData(0x44);
SPI_WriteData(0x04);

SPI_WriteComm(0xD2);
SPI_WriteData(0x00);
SPI_WriteData(0x43);
SPI_WriteData(0x64);
SPI_WriteData(0x25);
SPI_WriteData(0x10);
SPI_WriteData(0x02);
SPI_WriteData(0x71);
SPI_WriteData(0x44);
SPI_WriteData(0x04);

SPI_WriteComm(0xD3);
SPI_WriteData(0x00);
SPI_WriteData(0x43);
SPI_WriteData(0x64);
SPI_WriteData(0x25);
SPI_WriteData(0x10);
SPI_WriteData(0x02);
SPI_WriteData(0x71);
SPI_WriteData(0x44);
SPI_WriteData(0x04);

SPI_WriteComm(0xC2);
SPI_WriteData(0x08);
HAL_Delay(20);
SPI_WriteComm(0xC2);
SPI_WriteData(0x18);
HAL_Delay(20);
SPI_WriteComm(0xC2);
SPI_WriteData(0xB8);
HAL_Delay(20);
SPI_WriteComm(0xB5);
SPI_WriteData(0x01);
HAL_Delay(20);
SPI_WriteComm(0x29);
HAL_Delay(20);

}

 

 

This topic has been closed for replies.
MNapi
MNapiBest answer
Senior II
November 9, 2024

This is not the first time I am having problem to send data over SPI, that was the problem again.

You would have to see on logic analyzer to compare the waves.

So I disabled SPI and assigned PINs as output. And I made my own SPI interface using pins as output. And it worked fine, the display is initializing and working.

 

void SPI_SendData(unsigned char i)
{
unsigned char n;

for(n=0; n<8; n++)
{
if(i&0x80) HAL_GPIO_WritePin(GPIOI, GPIO_PIN_3, GPIO_PIN_SET);
else HAL_GPIO_WritePin(GPIOI, GPIO_PIN_3, GPIO_PIN_RESET);
i<<= 1;

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);//_nop_(); _nop_();_nop_();_nop_();

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);//_nop_();_nop_();_nop_();_nop_();

}
}

 

If somebody has similar problem with initialization over SPI does not work that might be the solution.

Maybe somebody from STM can collaborate?

4 replies

mƎALLEm
ST Technical Moderator
November 8, 2024

Hello @MNapi ,

Please use </> button to share your code.. I've edited your post then.. 

Please refer to the tips on how to post a thread.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
MNapi
MNapiAuthorBest answer
Senior II
November 9, 2024

This is not the first time I am having problem to send data over SPI, that was the problem again.

You would have to see on logic analyzer to compare the waves.

So I disabled SPI and assigned PINs as output. And I made my own SPI interface using pins as output. And it worked fine, the display is initializing and working.

 

void SPI_SendData(unsigned char i)
{
unsigned char n;

for(n=0; n<8; n++)
{
if(i&0x80) HAL_GPIO_WritePin(GPIOI, GPIO_PIN_3, GPIO_PIN_SET);
else HAL_GPIO_WritePin(GPIOI, GPIO_PIN_3, GPIO_PIN_RESET);
i<<= 1;

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);//_nop_(); _nop_();_nop_();_nop_();

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);//_nop_();_nop_();_nop_();_nop_();

}
}

 

If somebody has similar problem with initialization over SPI does not work that might be the solution.

Maybe somebody from STM can collaborate?

Tesla DeLorean
Guru
November 9, 2024

>>Maybe somebody from STM can collaborate?

Work with your account's FAE (support enginer), or other engineers on your team.

>>If somebody has similar problem with initialization over SPI does not work that might be the solution.

Probably timing or edge/phase configuration issues.

Check controller data sheet about expectations for CS, and data timing expectations.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..