Skip to main content
chrkaras
Associate III
Oct 31, 2025 1:27 AM UTC
Solved

DMA and PWM input mode/HRTIM output

Hello guys,

I have a stm32G474RET board. I am using tim1 in PWM input mode and i want to update on the fly the hrtimA period and compare values using DMA. 

This is the code i have written:

	// Addresses for HRTIM registers (Timer A)
	destPER = (uint16_t*)&HRTIM1->sTimerxRegs[HRTIM_TIMERINDEX_TIMER_A].PERxR;
	destCMP = (uint16_t*)&HRTIM1->sTimerxRegs[HRTIM_TIMERINDEX_TIMER_A].CMP1xR;

	// Start DMA transfers in circular mode
	HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_1, destPER, 1);
	HAL_TIM_IC_Start_DMA(&htim1, TIM_CHANNEL_2, destCMP, 1);

	HAL_HRTIM_WaveformOutputStart(&hhrtim1, HRTIM_OUTPUT_TA1);
	HAL_HRTIM_WaveformCounterStart(&hhrtim1, HRTIM_TIMERID_TIMER_A);

	HAL_TIM_IC_Start(&htim1, TIM_CHANNEL_1);
	HAL_TIM_IC_Start(&htim1, TIM_CHANNEL_2);

My problem is that the period of the hrtim is changing dynamically based on the input PWM signal, but the CMP1 doesn't. The only thing I could find is that when i tried to configure the channel 2 of timer 1 with DMA the CubeIDE didn't appear the TIM1_CH2 option, so it doen't "export" the value and thus this is the reason that it won't update the CMP1 of hrtimA.

I then tried by configuring the CH1 as direct input/rising edge and CH2 as indirect input/falling edge and while the TIM1_CH1/TIM_CH2 options appeared in the DMA configure tab, the CH2 after all reads the period of the 2 sequential falling edges.

My questions are:

1) Is there a way to manually add to channel2 the DMA configuration while in PWM Input mode?
2) If the (1) isn't possible, can you suggest any good way to sample a PWM signal without the PWM Input mode, but not either using the cpu(meaning to not need to subtract the CH2 - CH1 and then use DMA to update CMP1)?

Please, let me know if I can provide you with more information about my configuration. 

chrkaras
chrkarasBest answer
Associate III
Feb 12, 2026 12:00 AM UTC

Please, for anyone interested, refer to the following topic found here. 

1 reply

chrkaras
chrkarasAuthorBest answer
Associate III
Feb 12, 2026 12:00 AM UTC

Please, for anyone interested, refer to the following topic found here.